2026-01-23 9:16 AM
hello, I have a can bus with 2 node (one STM32G0B1 with SN65HVD1050DR transcriver and one esp8266 with
static void MX_CAN_Init(void) {
hcan.Instance = CAN1;
hcan.Init.Prescaler = 2;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_11TQ;
hcan.Init.TimeSeg2 = CAN_BS2_6TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = DISABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = DISABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK) {
Error_Handler();
}
/* USER CODE BEGIN CAN_Init 2 */
CAN_FilterTypeDef canfil;
canfil.FilterBank = 0;
canfil.FilterMode = CAN_FILTERMODE_IDMASK;
canfil.FilterFIFOAssignment = CAN_RX_FIFO0;
canfil.FilterIdHigh = 0x0;
canfil.FilterIdLow = 0x0;
canfil.FilterMaskIdHigh = 0;
canfil.FilterMaskIdLow = 0;
canfil.FilterScale = CAN_FILTERSCALE_32BIT;
canfil.FilterActivation = ENABLE;
canfil.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan, &canfil) != HAL_OK)
{
Error_Handler();
}
}
volatile uint16_t msgcount = 0;
uint8_t canRX[8] = { 0, 0, 0, 0, 0, 0, 0, 0 };
CAN_TxHeaderTypeDef txHeader;
uint32_t canMailbox;
int main(void) {
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_CAN_Init();
if (HAL_CAN_Start(&hcan) != HAL_OK)
{
Error_Handler();
}
if ( HAL_CAN_ActivateNotification(&hcan, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
Error_Handler();
}
txHeader.DLC = 8;
txHeader.IDE = CAN_ID_STD;
txHeader.RTR = CAN_RTR_DATA;
txHeader.StdId = 0x030;
txHeader.ExtId = 0x01;
txHeader.TransmitGlobalTime = DISABLE;
uint16_t delay = 500;
while (1) {
/* USER CODE END WHILE */
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_13);
uint8_t csend[] = {0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08};
if (HAL_CAN_AddTxMessage(&hcan,&txHeader,csend,&canMailbox) != HAL_OK)
{
Error_Handler();
}
if (msgcount > 0) {
delay = 100;
}
HAL_Delay(delay);
}
}
void incrementMessageCount() {
msgcount++;
}
CAN_RxHeaderTypeDef rxHeader;
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan1) {
HAL_CAN_GetRxMessage(hcan1, CAN_RX_FIFO0, &rxHeader, canRX);
incrementMessageCount();
}
Solved! Go to Solution.
2026-01-23 12:54 PM
turned out it was a transcriver issue, one pin on transcriver board was not soldered well. Sorry
2026-01-23 12:54 PM
turned out it was a transcriver issue, one pin on transcriver board was not soldered well. Sorry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.