STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431C + ADC + DMA

I'm using ADC with DMA in a large project, and faced some very strange problem: If I'm using DMA2 Channel 6 - ADC works correctly If I'm using DMA2 Channel 1 - the SW end up in Hard Fault The configuration is default. This is how I start the conversa...

Screenshot 2025-10-07 125752.png Screenshot 2025-10-07 125821.png Screenshot 2025-10-07 124405.png
AChas.1 by Associate II
  • 785 Views
  • 6 replies
  • 2 kudos

[STM32G0B0] External interrupt

Dear, I'm using a STM32G0B0RET6 as MCU and I encouter a bug on GPIO external interrupt specifically on PC14. Configuring as external IT on rising edge, it works correctly and the interrupt is generated only on rising edge.Configuring as external IT o...

YDann.7 by Associate III
  • 392 Views
  • 4 replies
  • 0 kudos

Resolved! Comparator Bug Report on STM32G0

I have configured the comparator 2 PB6 on the STM32G071RB Nucleo board. It is configured for rising edge interrupt.  As soon as HAL_COMP_Start is called on the COMP you can see the EXTI rising edge interrupt flag immediately go high. (well not immedi...

Carl_G_1-1737394247861.png
Carl_G by Senior III
  • 3381 Views
  • 13 replies
  • 3 kudos

STM32F47VITX6 USB identifies but does not send data

I have an STM32F4227 that identifies its USB port to a host PC and all information looks correct but no data is sent or received. Looking with the debugger the microcontroller is running task scheduler but does not recognize messages being sent. Is t...

lbrendel by Associate II
  • 334 Views
  • 3 replies
  • 1 kudos

STM32F427VITX RTC Init Fails with Timeout

During RTC init when RTC_EnterInitMode is called a unit sets the INIT bit of the RTC_ISR register in the HAL but when it waits for the bit set to respond it times out with the bit never being set. I have run this same firmware on hundreds of other un...

lbrendel by Associate II
  • 295 Views
  • 3 replies
  • 0 kudos

STM32 internal reference voltage configuration

Hi,I am working with STM32G491RET6 and currently implementing the ADC. I have a question regarding the ADC reference voltage.If the external 3.3 V supply is removed from the VREF+ pin and VREFBUF is disabled, does the ADC operate using any internal r...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.