STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error in the init of ethernet

 Good morning everyone!I'm working on a project involving FreeRTOS, lwip, and Ethernet with the ST32H563VGT6 MCU on a custom PCB.I'm attaching the hardware schematics, which we've taken from ST's schematics of the NUCLEO-H563ZI board. I'm including a...

Esquematicos_ETH.png JonConesa_0-1713435865970.png
JonConesa by Associate III
  • 9221 Views
  • 10 replies
  • 2 kudos

Resolved! internal resistance ADC

Good morning. I am working with the Discovery kit with STM32H7B3LI MCU and want to get its internal resistance. I want to use 10 buttons, each with one resistance, and then get the correct value for my MCU. I already know how to get the values betwee...

Capture d’écran 2025-02-01 à 16.02.36.png Capture d’écran 2025-02-01 à 16.03.23.png Capture d’écran 2025-02-01 à 16.03.44.png
Jad by Senior
  • 2155 Views
  • 3 replies
  • 0 kudos

Query: STM32F4 programming with USB

I can program my bespoke board using a repurposed USB port. It would normally be used by a mouse.I was under the impression that if I powered up the board with BOOT0 pin held high the MCU would be in a state to connect to USB and do it's enumeration....

Mike xx by Associate III
  • 2532 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F756 Ethernet and lwIP LWIP_RAM_HEAP_POINTER

I am using the latest version of CubeIDE (1.17.0), a STM32F765 Nucleo board with Ethernet. I am configuring the project to run lwIP using the internal Ethernet MAC. I am using FreeRTOS (CMSIS V2). CubeMX configures this LWIP_RAM_HEAP_POINTER to a def...

avinash_elec_0-1738381879008.png

SPI DMA is not workng at higher SPI baud rates

Hi,My NUCLEO-H563ZI application uses SPI with DMA. The SPI transactions are not working at clock/2 clock/4 and clock/8 rates, clock being 250 Mhz. Is there any clock frequency restriction when SPI is used with DMA? 

WCarey_0-1713875592886.png
WCarey by Associate III
  • 2436 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.