2023-12-13 1:22 AM
I read in the doc for the G431:
"The Flash main memory programming sequence in standard mode is as follows:
1. Perform a mass erase. If not, PGSERR is set."
So i can not do a single page erase??
Solved! Go to Solution.
2023-12-13 2:33 AM
Hello @Tobe ,
Yes, the fast programming mode can be performed just after a mass erase, if not, PGSERR (Programming Sequence Error bit) is set.
PGSERR bit: Programming Sequence Error is set in fast programming mode when the mass erase is not performed before setting FSTPG bit (Fast programming bit).
For more information please refer to Programming errors.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-13 2:33 AM
Hello @Tobe ,
Yes, the fast programming mode can be performed just after a mass erase, if not, PGSERR (Programming Sequence Error bit) is set.
PGSERR bit: Programming Sequence Error is set in fast programming mode when the mass erase is not performed before setting FSTPG bit (Fast programming bit).
For more information please refer to Programming errors.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-25 5:29 AM
Hello @Tobe ,
If you need any further clarification, please don't hesitate to ask.
If your question has been answered, please close this topic by choosing Accept as Solution. This will help other users find that answer faster.
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-31 5:21 AM
I would like to addend the question as my situation is similar
In order to protect my flash against uncomplete programming, my goal was to first do fast programming for all but the first page and after all pages are complete, I would program the first page with fast programming as well. When I do this, i always get PGAERR, PGSERR and FASTERR set as I lastly program the first page. Is there any way to mitigate this.
Best regards
Martin
2025-01-31 5:25 AM - edited 2025-01-31 5:27 AM
Never mind.
I can not delete post? Oh well....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.