STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

QUAD SPI External Memory Performance STM32

Hi There - I'm very new to electronic design and need help making a key design decision. Specifically I want to know that the performance will not be a problem when writing to external memory from a stm32 over Quad Spi. I don't want to end up making ...

AlanM by Associate
  • 8749 Views
  • 8 replies
  • 0 kudos

Resolved! GPIO Demo Program etc

Hello, can someone point me to where there are some demo programs for working with GPIO as individual pins and creating a bus from a number of outputs. I am also looking for a demo program with general s/w based timers, for example, in mbed which is ...

AndrewR by Associate II
  • 4035 Views
  • 7 replies
  • 2 kudos

Resolved! Enter low power run mode directly at boot

Hello community, I have this difficult task of powering an STM32G0B1 from a pin that was really not tasked for that (because the connector I have to plug onto provides no supply pin). In short, I can't draw more than 500µA current at any time or I ri...

WhatsApp Image 2025-01-28 à 11.17.07_4025050e.jpg
Kemsa by Associate II
  • 3818 Views
  • 9 replies
  • 2 kudos

Resolved! STM32H745 input fast read

Hi, I have problem. I have idea: my STM32H745 must read GPIO state as quickly as possible. FCPU = ~400MHzI wrote the program in assembler for M7LED_ON()ldr r2, [r3, #IDR]ldr r2, [r3, #IDR]... ~650xLED_OFF()...only read, IDR, no write (no record yet)A...

EsKi by Associate II
  • 2257 Views
  • 4 replies
  • 0 kudos

Resolved! STM32f411 crystal

Hi,I am new with stm32F411 mcu, and i have a question. if i want to use RTC features, do i need to add an external 32.768kHz xtal ?Thanks.

HL1 by Associate II
  • 1252 Views
  • 1 replies
  • 2 kudos

STM32WB55RG USART/LPUART unavailable?

Hello, I am trying to set up this is STM to connect it to another microcontroller via LPUART. To my understanding USART1 is unusable since it is connected to J-Link. I have attempted with LPUART setting up both PA3 and PA2 pins as the respective TX a...

STM32F4 with an ADAFRUIT BLE SPI

Hello st community,I'm trying to set up a bleutooth communication between my phone and my stm32 with the Adafruit module in SPI communication, but I'm having a problem.When I use my arduino and the demo code it works perfectly but when I connect to m...

Capture d'écran 2024-12-11 120927.png
Paulo971 by Associate III
  • 14823 Views
  • 21 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.