STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

No DFU detected, usb device not recognized code 43

I am trying to create a custom keyboard, and I was trying to flash my board with stm32f070c6t6 MCU in DFU mode using cube programmer, but I keep getting "no DFU detected" (of course while pulling BOOT0 pin high).Also, every time I plug my device into...

Screenshot 2025-01-16 at 3.06.15.png
HaYa6174 by Associate III
  • 9868 Views
  • 26 replies
  • 5 kudos

Resolved! Internal Pull up STM32G4 series

Hello,I am using the internal pull up for the input pins, but when read the port status using the program, it always reads 0 instead of 1. I expected it to read 1 and if make that pin grounded it shall read 0.   

STUser34 by Associate III
  • 4580 Views
  • 12 replies
  • 4 kudos

STM32H747: Reducing standby mode current consumption

Hello, We are using the STM32H747AI on a custom board and attempting to enter standby mode for power savings. The system supply is configured as "SMPS supplies LDO (no external supply)" to be able to use the boosted performance at 480MHz, but the chi...

2025-02-03T14_35_13,582544216+01_00.png
RopApe by Associate
  • 1519 Views
  • 2 replies
  • 0 kudos

Resolved! RM0477 Reference manual documentation error

Hello STM, I'm working on a project using the STM32H7R3L8H6H MCU with a PSRAM chip connected via HEXASPI to XSPM1. I'm encountering massive issues with the PSRAM initialization, which I described in a different post. I found a discrepancy between the...

Intector_0-1737788347282.png Intector_1-1737788477897.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.