STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! While(1) Not Executing

I am using STM32 with the following peripherals:TIM7 for frequency generationADC with DMADAC with DMATIM Interrupt (TIM_IT)My setup:Clock: 150 MHzPrescaler (PSC:( 3-1Auto-reload register (ARR:( 13-1128 samples for DAC to generate a 30 kHz signalWhen ...

controller getting restarted

Dear ST Community,I have been working on the firmware which contains the AT commands modem, Winbond flash memory. After some time I have relised the microcontroller is automatically getting restarted/. I had doubt on the hardware then  we have redeve...

Resolved! STM32U585 CLOCK JITTER

Dear Sir.I am using a board equipped with STM32U585 , The main clock is 32.768 khzsee included pic.PA8 is configured to drive LSE 32KHZ using the command__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_HIGH);PA8 is fed to ECG MAX30001.On some boards MAX30001 r...

Resolved! STM32L152RE 5V tolerant pin and ADC

Hello,I have a STM32L152RE and I use PA1 (Pin type is FT 5v tolerant) as ADC_IN1. Vdd is 3.3V and the voltage on PA1 usually is around 5V and sometimes it drops to 2.5V ( when I need to take the measure). Several comments on various blo...

RStra by Associate III
  • 9383 Views
  • 7 replies
  • 2 kudos

STM32G474 boot

Hi, I have a STM32G474 connected to a Quectel LTE module via a uart4 and a GPIO pin.Under normal conditions is it possible for the CPU to boot from flash and when the quectel changes the level of the gpio pin of the STm32, the CPU jump to boot from u...

bestyeng by Associate II
  • 3921 Views
  • 1 replies
  • 1 kudos

Resolved! Setting GPIO high does not work

I have created my first PCB with a STM32C011F6P6 on it, but I am not able to measure a GPIO I set high from my testpoint.I am setting PB6 high the following way:I flashed the code to the MCU via the cube ide and it told me that everything went fine.T...

DavidL__0-1738698244667.png DavidL__1-1738698255326.png DavidL__2-1738698326294.png
DavidL_ by Associate III
  • 1041 Views
  • 1 replies
  • 1 kudos

Resolved! RM0394 REV5 error

The link on the bottom of page 158 is bad.There is no SBF flag in PWR_CR3, actually it is in PWR_SR1.     

PSzab1_0-1738697510555.png PSzab1_3-1738697825111.png PSzab1_1-1738697643438.png
PSzab.1 by Associate II
  • 780 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H753 SVD File FDCAN Discrepencies

I downloaded the STM32H753 SVD file from https://www.st.com/resource/en/svd/stm32h7-svd.zipI have found a number of discrepancies between this file and RM0433  (reference manual)That leaves me wondering if this file is outdated and a more recent, cor...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.