STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBX CDC for the stm32u5 in standalone (no RTOS) problem

Hello,I implemented a virtual com port using the usbx stack for the stm32U575 in standalone mode and it basicaly works.My problem is that I just can't put more than 8 bytes in the TX buffer at the time. If I do the program gets stuck (in the main loo...

ckoec by Associate II
  • 2003 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 Peripheral lock (STM32h755)

I am working on an  application where I plan to relocate all non-safety modules to the CM4 core. To achieve full safety, I need a mechanism to lock the peripherals so that the CM4 core cannot access any peripherals configured in the CM7 core, includi...

sarun by Associate III
  • 1642 Views
  • 3 replies
  • 1 kudos

assembly code analysis

Can anyone comment on the prologue and epilogue of following CM7 code, particularly the content of r7 when the routine returns?   { 0: b480 push {r7} 2: af00 add r7, sp, #0 if ((ANADIG_MISC->MISC_DIFPROG & ANADIG_MISC_MISC_DIFP...

Observing a data shift in SPI receiption

Hi Team,I am observing a shift in a data each time i am sending same data from ESP8266 master to STM32f103RCT6 slave controller but each time i am getting different data and seems to be the shifted data as i can see some part of strings sent. I have ...

AADESH by Associate II
  • 2679 Views
  • 4 replies
  • 0 kudos

Resolved! writing flash memory failure

Hi everyoneI'm using a STM32F401RCT6 to control a valve actuatorThere is a counter of number of cycles for the actuator (RunTime), and when its value changes, the value of that counter must be stored in the memory for tracking and support.The actuato...

Resolved! Troubleshooting bricked Discovery STM32H745I board

I tried flashing a project created for the STM32H745I-DISCO board in CubeMx. The only change I made was disable a few unused peripherals, enable memory caching. I set the clock speed for the M7 core to 480MHz and the M4 core speed to 240MHz. I add...

Resolved! Timer 1 Retriggerable One-Pulse Mode

Hi, I want to do something extremely basic. Trigger a pulse using software for Timer 1 which is configured in Retriggerable One-Pulse Mode. Background: I can do the above if the Timer 1 is in normal One-Pulse mode. By simply Writing the CEN bit in TI...

danielbathtub_0-1738570289011.png danielbathtub_1-1738570680795.png danielbathtub_2-1738570759664.png danielbathtub_3-1738570915557.png

STM32F103C8T6 Firmware for Bootloader

Greetings to the community,I have a problem with creating a firmware for the bootloader. I'll start a little differently:Some time ago I made a bootloader for STM32F407VET6. The only thing I did was change the memory length in the STM32F407VETX_FLASH...

Chlaban by Associate
  • 1839 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.