STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Manchester encoding in low-end SM32s

Posted on May 11, 2018 at 11:18Are there any low-cost STM32 processors available which support Manchester encoding in the USART or similar?The Main processor will be a high-end STM32, but I need to bring some data across a 'difficult' isolation barr...

STM32F030R8 PA14 FOR Programming AND UART 2 TX

Posted on March 30, 2018 at 08:53Greetings All,I want to use PA14 for programming (which i am currently using) and after programming once controller resets i want to use same pin as UART 2 TX pin. How can i achieve this ?#stm32f030r8 #uart2

STM32L4 VDD vs VDDUSB vs VDDA

Posted on May 01, 2018 at 00:12I am designing with a STM32L4 in QNF48 and would like to save power...How about    VDDUSB = 3.3V    VDDA = 3.3V with linear regulator , VREF = VDDA    VDD = 1.8V     Now the data sheets say  |∆VDDx| must be less than...

STM32F030R8 and common anode 7 seg display

Posted on May 11, 2018 at 07:10Greetings People,I want to interface 6 common anode 7 segment display with my STM32F030R8. Any idea on schematic ?  I have interfaced it with 8051 but and i have used Max7219 with STM32F030R8.I don't want to go for Max...

Resolved! STM32F373 DFU bootloader won't start

Posted on May 10, 2018 at 22:27I have a STM32F373 design running with 16MHz HSE. My application works fine, but I am having trouble running the DFU bootloader. The host computer never sees a USB device. I have a previous F405 design using the same c...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.