2018-05-08 4:18 AM
Hi,
I am beginner in stm32 power supply 2.5v and Vdda 2.5
what is VDD_CALIB?
what is VDD_APPLI?
2018-05-10 8:32 AM
https://community.st.com/0D50X00009nNBAiSAO
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-05-10 3:54 PM
this is my code for the 'F091
#define TEMP110_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FFFF7C2)) // calibrated at 3.3V +-10mV @110C +/- 5C
#define TEMP30_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FFFF7B8)) // calibrated at 3.3V +-10mV @ 30C +/- 5C #define VREFINT_CAL ((uint16_t*) ((uint32_t) 0x1FFFF7BA)) // calibrated at 3.3V +-10mV @ 30C +/- 5C #define VDD_CALIB ((uint16_t) (3300))#define VDD_APPLI ((uint16_t) (3295))readtemp
double processorTemp; // the temperature in degree Celsius
int32_t AveTemperatureADC = ADC_Channel_AVE[VTemp_Ad16]; // 16x over sampled, needs /16
processorTemp = (double) AveTemperatureADC / 16 - *TEMP30_CAL_ADDR;
processorTemp *= 110 - 30; processorTemp /= ((double)*TEMP110_CAL_ADDR) - *TEMP30_CAL_ADDR; processorTemp += 30; processorTemperature = (int32_t)(processorTemp * 100); // sprintf(string,'AveTemperatureADC %04X, ADC_CalibrationFactor %04X, *TEMP30_CAL_ADDR %04X, processorTemperature %.2f, processorTemp %.3f \n\r',AveTemperatureADC,ADC_CalibrationFactor,(int32_t) *TEMP30_CAL_ADDR,((float)processorTemperature/100),processorTemp); // puts (string);Vdda = (double)16 * 3.3 * *VREFINT_CAL;
Vdda /= ADC_Channel_AVE[VRef_Ad17]; this works much much better after a calibrate. <- your next challenge.I get approx 30C at start and 38-43C running endlessly. usually 17C above ambient
2018-05-11 12:48 AM
hi,
thank you for your response
I need information about
VDD_APPLI and
VDD_CALIB if vdd 2.5v
2018-05-11 12:51 AM
what page in the reference manual are you on ?
2018-05-11 1:03 AM
hi,
referance manual stm32l071 RM0377 page no.847 and A.8.17 Temperature computation code example
not mention anywhere about
VDD_APPLI and
VDD_CALIB.
2018-05-11 1:44 AM
You need to find the voltage applied when calibrated in the datasheet.
3.12.1 Internal voltage reference (VREFINT)
The internal voltage reference (VREFINT) provides a stable (bandgap) voltage output for theADC and Comparators. VREFINT is internally connected to the ADC_IN17 input channel. Itenables accurate monitoring of the VDD value (when no external voltage, VREF+, is availablefor ADC). The precise voltage of VREFINT is individually measured for each part by ST duringproduction test and stored in the system memory area. It is accessible in read-only mode.Table 8. Internal voltage reference measured values
Calibration value name Description Memory addressVREFINT_CAL Raw data acquired at temperature of 25 °C 0x1FF8 0078 - 0x1FF8 0079 VDDA = 3 Vthat is
VDD_CALIB
= 3Vyour original question:
VDD_APPLI = 2.5V
.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.