2018-04-30 3:12 PM
I am designing with a STM32L4 in QNF48 and would like to save power...
How about
VDDUSB = 3.3V
VDDA = 3.3V with linear regulator , VREF = VDDA
VDD = 1.8V
Now the data sheets say |∆VDDx| must be less than 50mv .
Is this mean all power need to be at the same level +/- 50mv, or that all of the same name need to be within 50mv
Thanks!!!
2018-05-01 1:01 AM
Now the data sheets say |∆VDDx| must be less than 50mv .
Which datasheets? And how do they exactly describe what |∆VDDx| is?
JW
2018-05-01 3:55 AM
Every STM32 datasheet I ever saw.
So if this is true that all vdd need to be basically the same voltage
Can we use the USB while vdd is not 3.3V?
Thanks
2018-05-01 12:55 PM
Every STM32 datasheet I ever saw.
Show (you can paste pictures here).
JW
2018-05-11 12:03 AM
|∆VDDx| must be less than 50mv :- Variations between different VDDX power pins of the same domain
So if VDDIO2 ,VDD ,VDDUSB are of separate domains so no issue as of my knowledge correct me if i am wrong.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.