2018-05-11 2:18 AM
Are there any low-cost STM32 processors available which support Manchester encoding in the USART or similar?
The Main processor will be a high-end STM32, but I need to bring some data across a 'difficult' isolation barrier, and one very easy way to do this would be to have a cheap processor on the 'live' side of the barrier, measuring various things and streaming the data, Manchester encoded. This would mean I could use a low-cost, high spec pulse transformer to get all the data across the isolation barrier, at low power and high speed. For this application I do not need a return channel.2018-05-11 2:57 AM
Not that I'm aware of, the USART are of pretty simplistic design.
One might be able disabuse a 16-bit SPI shifter and some encode tables on the TX side
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.