2018-05-10 10:48 PM
On the stm32F3 discovery boards, where do pins on CN3 get connected when CN4 jumpers are on and off.
Schematics says, CN4 jumpers on, will select discovery. Off means ST-LINK is selected.
If I take CN4 off, then CN3 pin2 is not connected to PA14 of st32f303 device.
I have to have CN4 on for PA14 to get connected to pin2 of CN3.
Please help me.
Solved! Go to Solution.
2018-05-10 11:12 PM
The pins in CN3 always connect to the output pins of the ST-LINK STM32F103, CN4 connects the ST-LINK to the F3 target on the board.
If you want to program an external target STM32 via CN3 then you need to disconnect the on-board target by removing the CN4 jumpers. You do this so you don't have TWO targets with SWDIO/SWCLK pins that clash and cause it so neither can be programmed/debugger properly.
2018-05-10 11:12 PM
The pins in CN3 always connect to the output pins of the ST-LINK STM32F103, CN4 connects the ST-LINK to the F3 target on the board.
If you want to program an external target STM32 via CN3 then you need to disconnect the on-board target by removing the CN4 jumpers. You do this so you don't have TWO targets with SWDIO/SWCLK pins that clash and cause it so neither can be programmed/debugger properly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.