STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32l47

Posted on May 10, 2018 at 22:20hello, I have three identical electronic cards inculcate the chip stm32l47 and I raised the soft correspendant on these three cards via protocol uart but the problem what two functional cards and the other I have been ...

Problem of uart and usb stm32l47

Posted on May 10, 2018 at 22:18hello, I have three identical electronic cards inculcate the chip stm32l47 and I raised the soft correspendant on these three cards via protocol uart but the problem what two functional cards and the other I have been ...

How to get the unused flash location to use write

Posted on May 07, 2018 at 19:55 Hi , I was trying to write array of 10 element in to the flash. But it was writing to used code memory. I am using STM32F103C8T6 and keil compiler and code generated by cubemx. Here is my code. uint32_t...

SS.Sagar by Associate III
  • 3382 Views
  • 4 replies
  • 0 kudos

ST-LINK/V2 Pin Header

Posted on May 08, 2018 at 17:04Hello.I want to use theST-LINK/V2 to program a customSTM32F0microtroghtSWD.Taking a look atST-LINK/V2 User Manual(UM1075),I had a doubt aboutVAPPpins.Thesepins(1and2), are input or outputpins?I guess thesepinsare input...

0690X0000060B4SQAU.png

Generating PWM Waveform with STM32L011?

Posted on May 10, 2018 at 12:24Hi all,I'm new to using timers and I'm currently trying to generate a PWM Waveform so that I can use this to power some motors. At the moment I am testing the PWM Waveform via LED's rather than going straight to the mo...

Bug Report cubeMX 4.23 IAR code genereator

Posted on November 28, 2017 at 09:02HelloI use cubeMX 4.23 and have seen that the code generator for IAR itroduces absolute paths in the *.ewp project file in the include section and for all used library source files which are used in the project.I ...

F103 SDIO Init Problem

Posted on March 30, 2018 at 05:34The problem is when code run to HAL_SD_ConfigWideBusOperation(&hsd, SDIO_BUS_WIDE_4B), it always return HAL_ERROR.And then SD init failed and stuck in _Error_Handler function.MCU: STM32F103VETxCube MX Version: 4.25.0...

0690X00000604WUQAY.jpg
Zhi Pang by Associate III
  • 5275 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.