STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ETB on STM32F20x ?

Posted on May 22, 2018 at 10:41Asking more in hope than expectation really, but does anyone know if the STM32F20x (specifically, STM32F205RB) supports ETB?  J-Link doesn't report it;CoreSight components:ROMTbl[0] @ E00FF000ROMTbl[0][0]: E000E000, CI...

Connecting two image sensors to an STM32F69

Posted on May 24, 2018 at 11:13We're working on a project in which we've connected an image sensor to the STM32 DCMI.I'm now planning the next project, in which I want to connect two sensors, where only one should be active an any given moment, but ...

Unlock readout protection

Posted on August 28, 2017 at 11:43Hi Everybody,I have problem unlock readout protection with HAL library on STM32F030F4.My application need to apply lock / unlock by programming. The lock code works fine. After running lock code, RDPLevel shown in S...

CW Fu by Associate
  • 1426 Views
  • 1 replies
  • 0 kudos

Why mcu not reset on ESD test ?

Posted on May 16, 2018 at 08:54 When I run system clock through HSE(8MHz/24MHz/25MHz) and PLLCLK (multiplier PLLN and divider PLLM & PLLR) than mcu not reset by ESD.But when I run system clock directly through HSE(8MHz/24MHz/25MHz) than mcu get res...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.