2018-05-15 11:54 PM
When I run system clock through HSE(8MHz/24MHz/25MHz) and PLLCLK (multiplier PLLN and divider PLLM & PLLR) than mcu not reset by ESD.
But when I run system clock directly through HSE(8MHz/24MHz/25MHz) than mcu get reset by ESD.
Can any one comment for my issue..
Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-05-16 2:36 AM
Hello
Rana.Mahendra_Singh
,What is the Hardware board used ?
Best Regards
Imen
2018-05-16 3:47 AM
Board is design by our own
2018-05-16 6:55 AM
>>Board is design by our own
That's really not very illuminating.
The cue here is to provide more clear and specific information about the system that has a problem.
2018-05-16 7:01 AM
That board is not any nucleo board. Its circuit and pcb was designed by our own.
2018-05-16 7:06 AM
Ok, but this provides zero insight, to social cue here is to provide sufficient detail that someone not inside your head can understand/see what is going on.
Present your question with enough context that it might be reviewed.
Not sure how HSE vs HSE+PLL would behave materially differently in the current context. Is a reset response to a large ESD not a likely/acceptable outcome?
2018-05-16 7:08 AM
The cue here is to provide more clear and specific information about the system that has a problem.
And what is the problem at all.
At least for burst/surge tests which are required for commercial devices here, the DUT is allowed to stop operating during the test. It only must not sustain permanent damage.
2018-05-16 7:26 AM
My problem is :- During ESD test(contact discharge of 2KV/4KV and air discharge test upto 8KV) MCU got reset automatically when in code I run system clock through HSE ON(8/24/25 MHz) and PLL OFF. Means program counter also reset and starts from initial code.
But for same ESD test when I run system clock through HSE ON (8/24/25 MHz) and PLL also ON than MCU never resets. Why so?
Note :- Right now I am testing through electric lighter as not having ESD gun in my lab. But tested with ESD gun
when in code I run system clock through HSE ON(8/24/25 MHz) and PLL OFF and MCU got reset automatically that time.
2018-05-16 7:29 AM
No permanent damage only MCU reset and my HMI regain its same state so ESD test was passed in Type B category (IEC-61800-3 and IEC 61000-4-2).
2018-05-16 7:31 AM
My problem is :- During ESD test(contact discharge of 2KV/4KV and air discharge test upto 8KV) MCU got reset automatically when in code I run system clock through HSE ON(8/24/25 MHz) and PLL OFF. Means program counter also reset and starts from initial code.
But for same ESD test when I run system clock through HSE ON (8/24/25 MHz) and PLL also ON than MCU never resets. Why so?
Note :- Right now I am testing through electric lighter as not having ESD gun in my lab.
But tested with ESD gun
when in code I run system clock through HSE ON(8/24/25 MHz) and PLL OFF and MCU got reset automatically that time.
No permanent damage only MCU reset and my HMI regain its same state so ESD test was passed in Type B category (as per IEC-61800-3 and IEC 61000-4-2 standards).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.