2018-05-22 1:41 AM
Asking more in hope than expectation really, but does anyone know if the STM32F20x (specifically, STM32F205RB) supports ETB? J-Link doesn't report it;
CoreSight components:
ROMTbl[0] @ E00FF000
ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 002BB000 SCS
ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 002BB002 DWT
ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB
ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 002BB001 ITM
ROMTbl[0][4]: E0040000, CID: B105900D, PID: 002BB923 TPIU-Lite
ROMTbl[0][5]: E0041000, CID: B105900D, PID: 002BB924 ETM-M3
Cortex-M3 identified.
J-Link>etb
ETB is not present.
....and I don't see it in the datasheet either so I'm pretty sure I know the answer to my own question...but having gone to all of the trouble to include the ETM I'm sorta surprised there's no ETB there too....
DAVE
2018-05-22 5:20 AM
ETB means RAM that means silicon area and that means cost per chip.
Not having included it means only the negligible minority of users who want to trace bear the burden of spending pins and buying the exorbitantly expensive trace tools.
JW
2018-05-24 3:50 AM
Jan,
Thanks for the replyt, but I guess that's no then? :) Some vendors allocate the ETB RAM in a re-usable block so it doesn't need to be dedicated to ETB all of the time....that seems like a nice compromise - I can often forsake some function of my application while I'm trying to figure out how I'm in the hardfaultHandler...
(Oh, and I agree about price of the trace tools! The Orbuculum project is building free/Free alternatives, but it's a way off completion yet).
Regards
DAVE
2018-05-24 6:02 AM
Thanks for the reply, but I guess that's no then? :)
I'm not ST, but given what you've written and what's in DBG chapter of RM0033... Yes, no. :D
Some vendors allocate the ETB RAM in a re-usable block
In Cortex-M3/M4? Not that I couldn't imagine it, but I guess there are tradeoffs...
At the end of the day, this is just another tool in the developer's toolbox - and while it may be useful, it needs to be learned and taken care for too. During the years I've gradually learned to pay less and less attention to any particular debugging (or development for that matter) technique (and even less if it's been promoted loudly in the glossy material), as at the end of the day it's the complete mix which counts. YMMV.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.