STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F75xxx and STM32F74xxx Reference Manual Error ?

Posted on May 22, 2018 at 21:33In RM0385, Rev 7At the top of page 957, it states 'For I2C I/Os supporting 20 mA output current drive for Fast-mode Plus operation, the driving capability is enabled through control bits in the system configuration con...

STM32L053R8 PWM for 100MHz

Posted on May 22, 2018 at 08:38Hi,I am using STM32L053R8 controller.I want to generate 100MHz, with 50% duty cycle.Can you please share the code?#stm32l053r8 #stm32l053r8-nucleo

stm32f769 dsi application problems

Posted on May 23, 2018 at 04:41Dear:   I am working on STM32F769 development board with the dsi unit.   I set the dsi clk to non-continuous mode and set dsi to LP command mode.  Then I  inited  the dsi module and started the DSI calling the the func...

CAN Bus interrupt stopped working

Posted on May 24, 2018 at 03:42 Hello everyone, I am using STM32F072C8 with MAX3051 CAN BUS transceiver to gather CAN bus data from a vehicle. Below is the main part ofmycode. while (1) { main_counter++; sprintf(print_buf1, '\r\n%d | main_c...

stm32 lora

Posted on May 08, 2017 at 08:48Hi. I have to study the lora world with a stm32 microcontroller.For me it is the first approach. Can someone suggest me witch stm32 demo board is the most easy to use in order to learn how lora works?Can someone sugges...

Compile time is taking forever

Posted on December 18, 2017 at 20:18Hi Everyone.I recently updated my SW4STM32 IDE when prompted to do so from a pop up, and I'm now seeing its taking forever to compile a project. For example I cleaned one of my mailto:STM#@F0 Adafruit LCD shield d...

mbmail4 by Associate II
  • 1077 Views
  • 1 replies
  • 0 kudos

stm32 and jump to function

Posted on May 16, 2018 at 12:15Hi. Iì'm trying to implement the jump to function.So my stm32 microcontroller has got 2 firmwares.The first is located at address 0x08000000 and the second is located at address 0x08008800.Using the st flash utility I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.