STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hexapod robot with STM32F4 and Camera detect of objects

Posted on May 24, 2018 at 23:43good morning  people i'm newbie in this plataform and I need a little bit of your help, I'm doing a project of a hexapod robot but I want it to detect objects with a camera module and if it loses the object that looks ...

EEPROM Emulation for the STM32 CubeF1

Posted on January 17, 2018 at 17:37Hi,In the STM32Cube_FW_F1_V1.6.0 software package i found the EEPROM example. STM32Cube_FW_F1_V1.6.0\Projects\STM32F103RB-Nucleo\Applications\EEPROMCan someone tell me how the flash reservation is handle here? How ...

MSP430 information memory equivalent inside the STM32?

Posted on May 25, 2018 at 11:17Hello,Is there inside the STM32L476 a flash memory reserved to user parameters?This memory would be the equivalent of the information memory of the msp430 competitor.If no, can I use any sector of the code memory?Can I...

Mich1 by Associate III
  • 2006 Views
  • 3 replies
  • 0 kudos

STM32F032 CAN bus

Posted on May 18, 2018 at 12:01Turvey.Clive.002‌ Barkin.Tyler.001‌Hi Clive , I'm using the STM32F072 discovery board. In that i'm using the CAN peripherals CAN_Tx and CAN_Rx .Below is the circuit diagram of my connection. I'm using MCP2551 trans...

0690X0000060BHlQAM.png

Interfacing a Bluetooth Module with STM32L0xx

Posted on May 25, 2018 at 05:35Hello STM32 community,I'm working on a project to interface a Bluetooth module(Adafruit Bluefruit LE Friend) with STM32L073RZ. I'll be using HAL drivers and STM32CubeMX in this project. I'm new to STM32 environment. I ...

Ash G by Associate II
  • 962 Views
  • 0 replies
  • 0 kudos

HAL_UART_Receive() timeout issue

Posted on May 24, 2018 at 20:40Hi,I am using Nucleo-144 board connecting UART to my TI device using 250000 baudrate. I always got timeout no matter what timeout using.Seems the issue is UART_WaitOnFlagUntilTimeout() failed and return HAL_TIMEOUT.if(...

MOE behaviour on TIM1/8/20

Posted on May 09, 2018 at 16:39Hello forum,I am new to STM32 but familiar with programming DSPs/MCUs.I just bought a NUCLEO-F303ZE board and I am struggling with the PWM-Timer block. I have set up a CubeMX project and I achieved a project with a PWM...

stm32 m0 and firmware relocation

Posted on May 24, 2018 at 22:03According with the example these lines of code    #define APPLICATION_ADDRESS     (uint32_t)0x08004000    volatile uint32_t *VectorTable = (volatile uint32_t *)0x20000000;    uint32_t ui32_VectorIndex = 0;    for(ui32_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.