2018-05-24 2:13 AM
We're working on a project in which we've connected an image sensor to the STM32 DCMI.
I'm now planning the next project, in which I want to connect two sensors, where only one should be active an any given moment, but the switch between them must be fast (~100ms time to image).
My thought was to connect the sensors to two different sets of pins that can function as DCMI, and changing the pins configuration from GPIOs to DCMI and vice-versa according to need. This will save the need for muxs/switches, and I can have both sensors powered at the same time.
Does this sound reasonable? would the DCMI require a restart, or the entire MCU?
Thanks,
Yoel
2018-05-24 2:55 AM
DCMI runs around 300 - 500MHz
To switch lossless at those frequencies without crosstalk, these are not cheap switches.
H.264 over ethernet. would be my suggestion.
2018-05-24 5:53 AM
Thanks T J.
As I've mentioned I'm trying to avoid the use of switches of any kind. My goal is to work with the DCMI configuration only.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.