STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G4 not waking from STOP1

I am working on a project using an STM32G4. I have a new board spin that I am bringing up and one of the four boards that I have brought up is exhibiting strange behavior exiting STOP1 mode.I have code that can put the micro into one of 2 low power m...

matkSENS by Associate II
  • 1255 Views
  • 2 replies
  • 0 kudos

QSPI Data Transfer between MCU and FPGA

  I have designed a PCB that connects an Artix-7 XC7A35T-1FTG256C FPGA with an STM32F469VET6 (LQFP 100) MCU. My goal is to transfer data between these two devices, with the MCU as the QUADSPI master and the FPGA as the slave. For communication, all Q...

Resolved! STM32F405RGT6 and CAN not working

I try to get the CAN working. But currently I'm not sure what I'm missing.I use the STM32CubeIDE v1.18.0. The boards I use is own hardware with SN65HVD232.The hardware seems to work well. on the picture you see the screenshot from my oscilloscope, CA...

Resolved! STM32F411 Bootloader hangs

Hi there!I've created a custom STM32F411CEU6 Board with external HSE und LSE. While the HSE works when running my user program, the Bootloader hangs within boot phase (i think).When starting bootloader, BOOT0=1 und BOOT1=0. I powered direcly on VDD, ...

Gifford_0-1742722709972.png Gifford_1-1742722726214.png Gifford_2-1742722747432.png Gifford_3-1742722763253.png
Gifford by Associate II
  • 4961 Views
  • 13 replies
  • 0 kudos

How to read the volume keys from a USB keyboard

I've read many posts here and on the web, even tried CoPilot, but I could not find how to get the USB controller to send data when the volume keys are pressed.My Host keyboard driver works perfectly, but USBH_LL_GetURBState() is not returning with da...

Robmar by Senior III
  • 3014 Views
  • 7 replies
  • 1 kudos

Resolved! FDCAN1 not working on PA11 and PA12

Hello everyone, I tried to put Canopen node for stm32 into operation. I used the standard pinning from STMCubeIde, i.e. pa 11 and 12. But this does not seem to work. void FDCAN1_IT1_IRQHandler(void) { /* USER CODE BEGIN FDCAN1_IT1_IRQn 0 */ /* USER ...

Meiko_Ju by Associate II
  • 6906 Views
  • 14 replies
  • 1 kudos

Resolved! QuadSPI and BOOT1 with STM32F446RET6

I'm trying to interface the STM32F446RET6 with M95P32-IXCST/EF, a QuadSPI EEPROM. For the 64 pin STM32F446RET6 pin PB2 (pin 28) is used both as BOOT1 and QUADSPI_CLKI don't see any other pins that can be used as QUADSPI_CLK for the 64 pin package. Is...

SBat_0-1742973353678.png
S-Bat by Associate II
  • 1641 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H755Zi-Q~How to share data between cores

Currently I am just trying to share some data between cores, and right now I'm just trying to send a constant value to confirm operation.I have this code located in a file called share.h,typedef struct {   // shared data goes here   int16_t data;   }...

CFran.1 by Associate II
  • 4695 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G0B1RC LSCO output on PA2 even the LSCOEN=0

Started using PA2 pin as a ADC input and found that the input voltage get corrupted with LSCO output. Happens not always, but very often. Powering board down and up sometimes fixes the problem, sometimes not.The LSCO output enable control bit LSCOEN ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.