2021-04-22 11:57 AM
Currently I am just trying to share some data between cores, and right now I'm just trying to send a constant value to confirm operation.
I have this code located in a file called share.h,
typedef struct {
// shared data goes here
int16_t data;
}shared_data_t;and then I have
volatile shared_data_t * const shared_data = (shared_data_t *)0x30040000;saved in each core's main.c file.
The location is SRAM3 and according to the RM this is an optimal place to share values. It updates properly in M7, but when I check the struct in M4 it's not the same value. When googling, this was the number 1 answer, the second was the linker. I don't know where to begin with the linker, so if that is the option is there any good guides? Thank you for reading this
Solved! Go to Solution.
2021-04-27 6:09 AM
Hi @CFran.1 ,
The application note AN5617 STM32H745/755 and STM32H747/757 lines inter-processor communications is meant for use-cases as yours.
It provides an overview of the dual-core communication technique & introduces the inter-processor communication channels such as OpenAMP, RPMsg, FreeRTOS as well as the message buffer and custom communication mechanism (with some code snippets).
This is a new document, don't hesitate to share with us any feedback about its content.
-Amel
PS: Once your question is answered, please click on "Select as Best" for the comment containing the answer to your initial question.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-04-22 12:14 PM
volatile isn't sufficient for cache coherency.
Perhaps use the MPU memory settings, fencing instructions, or Clean DCache type functionality to ensure the memory is consistent.
There is also the HSEM peripheral
2021-04-22 12:27 PM
Thank you for the reply. I am currently using HSEM
//M7 Main File
while(HAL_HSEM_FastTake(HSEM_ID_0)){}
shared_data->data = 0x69;
HAL_HSEM_Release(HSEM_ID_0, PID_ID_0);//M4 Main File
while(HAL_HSEM_FastTake(HSEM_ID_0)){}
HAL_HSEM_Release(HSEM_ID_0, PID_ID_0);I use a breakpoint at the M4 HSEM_Rlease to ensure the M7 is polling.
When I'm in the breakpoint, I'm using the debugger watch-variable to watch shared_data->data in the M4 file
2021-04-22 3:21 PM
I came across the https://www.st.com/resource/en/application_note/dm00272913-level-1-cache-on-stm32f7-series-and-stm32h7-series-stmicroelectronics.pdf, and it makes sense why my data is getting stuck in the D-cache. Thank you!
2021-04-27 6:09 AM
Hi @CFran.1 ,
The application note AN5617 STM32H745/755 and STM32H747/757 lines inter-processor communications is meant for use-cases as yours.
It provides an overview of the dual-core communication technique & introduces the inter-processor communication channels such as OpenAMP, RPMsg, FreeRTOS as well as the message buffer and custom communication mechanism (with some code snippets).
This is a new document, don't hesitate to share with us any feedback about its content.
-Amel
PS: Once your question is answered, please click on "Select as Best" for the comment containing the answer to your initial question.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-26 2:29 AM
Now, I am using the NUCLEO-H755ZI-Q board, and I am stuck on the same problem. I think you already have the answer. Could you share how to solve the issue of using the same (shared) variable in across different cores?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.