STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! fdcan bit time config for classic frame STM32H563VGT6

Hi,this is myproduct code STM32H563VGT6. I am configuring the FDCAN2 module.In particular the bit time using the filed below of the init structure of the HAL handler:hfdcan2.Init.NominalPrescaler (NBRP+1 of register FDCAN_NBTP)hfdcan2.Init.NominalSyn...

DAUSILI by Associate III
  • 4205 Views
  • 6 replies
  • 2 kudos

STM32H562RIT6_temperature sensor

HiWhat is the exact percentage error of the internal temperature sensor in the STM32H562RIT6 microcontroller?Is this error percentage consistent across all temperature ranges?Please provide the exact percentage error for different temperature ranges....

Resolved! Cube MX bug about DSP

Hi everyone;I have select;In cube mx -> middleware and software packs -> X Cube Algobuild -> DSP LibraryHowever , there is no dsp libraries in my keil project.And there is no .lib in the folder.I have re-generate for several times, but it did not tak...

Neeee by Associate
  • 1293 Views
  • 2 replies
  • 3 kudos

I2S bits rotated

HiI am working on project that receive several I2S streams from MEMS microphones. I found that "audio level" from second microphones pair had higher level then from other. After some analysis and SD lines swapping i found that I2S data received by se...

i2s_SD-0xAAAAAAAA_CK.png i2s_SD-0xAAAAAAAA_WS-fall.png i2s_SD-0xAAAAAAAA_WS-rise.png i2s_WS-fall_CK.png
max_verem by Associate II
  • 3226 Views
  • 9 replies
  • 0 kudos

Resolved! STM32L452 LSE not starting

I have an STM32L452 rigged to use an external clock so we can keep the RTC running. Schematic attached.X2 is a clock from SiTime, programmed to be 32.768kHz. C36 is a supercap acting as battery backup. I used STMCube to generate the startup code to f...

LSE_schem.png
SLevi.1 by Senior
  • 9298 Views
  • 18 replies
  • 2 kudos

Resolved! LTDC not starting STM32H7S7Z8J6

Hi, Currently we have received our first prototype batch of board with the STM32H7S7Z8J6. There is external flash and ram on the board also, but first we want to try a simple test where we will just use the LTDC interface without touchgfx to make the...

leddel32 by Associate II
  • 2185 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.