STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32F072CBT6 versus Stm32F072C8T6

hello. I was using PA9 pin as an interrupt in a project made with Stm32F072CBT6. I am working as Stm32F072CBTx in cubeide. The card I am working on accidentally installed Stm32F072C8T6. only difference is that it is visible in flash but PA9 pin can b...

IMP34DT05TR Mic Read issue...

Hi,I am trying to interface the IMP34DT05TR microphone with our custom board. After soldering with custom board, we are unable to read data from the microphone, and the sample data appears incorrect. data look like this when open the audio file in no...

kri_srushty_1-1743072201926.png ImportedPhoto_1743070830681.jpg ImportedPhoto_1743070679567.jpg

Resolved! Counter using hrtim

Hii, I am using hrtim in stm32G474RET6 mcu, so i want to know how we generate a counter of 500ns in which i call adc in it.If somebody know about it please help me.

Harsh_18 by Associate III
  • 2963 Views
  • 7 replies
  • 1 kudos

Resolved! wake up from standby mode U545REQ

Hi, I set the button on the board to WAKE_UP2 to wake up from standby mode, but it doesn't work. Also, waking up through the RTC interrupt doesn't work either. The LSE source is an external crystal. This is my code: int main(void) { /* USER CODE BEG...

dlagyals by Associate II
  • 1167 Views
  • 1 replies
  • 0 kudos

How to implement USB DPM, prevent hard reset

I tried following STM32 AN5418 but the EvaluateSinkCapabilities method is not getting called. I added debug prints everywhere in the code and here is what I am receiving:1. VBusInit (this always happens)2. DPM notification 104 (Stack init)3. Cable de...

Nv7 by Associate III
  • 1779 Views
  • 3 replies
  • 0 kudos

Is there a guide on how to use I2C with DMA?

Bonjour,I've been able to use I2C to communicate with I/O extender and display drivers with HAL. I'm now trying to use the I2C with HAL using DMA.The problem is that UM1785 Description of STM32F0 HAL and low-layer drivers is a bit vague on explanatio...

Matth1 by Associate III
  • 29866 Views
  • 6 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.