STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_FLASH_Program does not support programming bank 2

When trying to program the STM32L4P5RE, I get an assertion failure when trying to program the second bank like this:HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, address, data)This call fails if my address is in the second bank `0x08080000`.  Looki...

dcooperch by Associate II
  • 1269 Views
  • 2 replies
  • 2 kudos

Resolved! CAN communication not working F407 with G431

I have two Nucleo boards that are connected with a CAN bus (Transceiver SN65HVD230). I would like to communicate with standard CAN, eight data bytes, data rate 50000 bit/s. For the F407 all TX & RX events are triggering (reused old working code) the ...

CubeMX_F407.PNG CubeMX_G431.PNG

Resolved! STM32U575: Understanding RCC::CSR reset bits

I'm trying to understand how the CSR register works. I though initially that the various reset reason bits are mutually exclusive. That turns out not to be the case. For example, I'm seeing SFTRSTF and PINRSTF together, and also BORRSTF with PINRSTF....

USB Audio class

Hi,I am using nucleo-l476RG board.I am new to USB audio, I am trying to create USB Audio class (Speaker/MIC) using HAL. I am sucessfully able to create a node for speaker and MIC in my laptop. But unable to send and receive the data over USB. Can any...

f_mount() error on STM32H750VBT6

I have WeAct studio's STM32h750VBT6 board. i am trying to access Sandisk's 64 GB MicroSD card (formatted as FAT32) through MicroSD card Adapter using SPI1. I am not able to access memory card. i have enable SPI1 and made enable PB1 (SD_CS) as gpio_ou...

Prajyot1_0-1746593407031.png

Resolved! Debug Options on C091 Custom Board

I made a custom board using a C091KCT6. I assumed I would be able to figure out a way to display data in real time using printf. Unfortunately, I did not make provision to expose PA2 and PA3 (or indeed any pins other than the ones used by my board). ...

Resolved! HAL_RTCEx_BKUPWrite

Hallo, the information written on rtcbackup register, is retained when micro is powered off?Or the information will be lost?

IVent.1 by Senior
  • 1080 Views
  • 1 replies
  • 0 kudos

Getting wrong ADC readings

Split from:https://community.st.com/t5/stm32-mcus-embedded-software/how-to-use-analogue-pins-not-adc-to-read-voltage/td-p/792208Please keep to one question per thread.Hi, One more related question, I have changed the pins and now i am reading the vol...

sal92 by Associate II
  • 2369 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.