STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No device found on target. After some succesfull uploads

Hi,I am working with a custom board with the STM32L431CCU6 mcu. The bord consist of the mcu and 2 i2c units and one SPI.The board also has pin headers for BOOT0, SWDIO and SWCLK.Sory for paint... I am using the CubeIDE and a ST-LINK V2for programming...

assjo_1-1746535632587.png assjo_2-1746537392875.png
assjo by Associate II
  • 1705 Views
  • 2 replies
  • 2 kudos

Resolved! How to configure "Delay between 2 sampling phases" on the STM32G431

板:STM32G431 NUCLEO-64我的目标是在 ADC1 和 ADC2 上实现 4 MSPS 的采样率。通过使用交错采样,我的目标是获得 8 MSPS 的有效采样率。虽然我知道这可能与数据表中针对多通道 ADC作的声明限制不严格一致,但我相信这种差异与我遇到的问题没有直接关系。根据数据表中的图1、ADC 时钟应低于 52 MHz。图 1在我的设置中,我在交错模式下使用 TIM + DMA + ADC,配置如下:定时器触发频率:4 MHzADC 分辨率:12 位ADC 时钟:60 MHz采...

Clavinz_2-1746070306442.png Clavinz_3-1746070369648.png Clavinz_4-1746070376305.png Clavinz_5-1746070389460.png
Clavin-z by Associate
  • 2525 Views
  • 2 replies
  • 0 kudos

DSI issues driving a SN65DSI86

Dear forum mmebers,I am trying to use an STM32U5G9 MCU to drive a Ti SN65DSI86 DSI to eDP converter with no success.Previously I have evaluated the SN65DSI86 with a Xilinx FPGA as a DSI source where it was working perfectly from 640x480 to 1920x1200 ...

balint by Associate II
  • 14205 Views
  • 8 replies
  • 0 kudos

Resolved! STM32F769 VDDUSB

Hello,I'm using in my projects with ports PA10,PA11 (for Logs - uart), and PB14 and PB15 as normal GPIO.They didn't works.After long troubleshooting.... I found out that is because these ports are supply separately by the VDDUSB pin which was disconn...

UB40 by Associate
  • 1383 Views
  • 2 replies
  • 1 kudos

Resolved! STM32L031 noisy, even in reset - EDIT: it's not the STM32

EDIT: it's not the STM32, see latest postHeyho,I have some custom miniature PCBs here, the unholy combination of a super-high-impedance-low-noise amplifier (going to a low noise audio input with 24bit ADC, spectra below from that one) and a STM32L031...

Amp_Noise_MCU_removed.png LCE_0-1742313100646.png LCE_1-1742313120753.png
LCE by Principal II
  • 4453 Views
  • 9 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.