Development kit for STM32F407VET6?
Anyone who knows that Development kit for below given part number(Connect D[7:0], PCLK, HSYNC, and VSYNC), and Can we video streaming via USB?STM32F407VET6.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Anyone who knows that Development kit for below given part number(Connect D[7:0], PCLK, HSYNC, and VSYNC), and Can we video streaming via USB?STM32F407VET6.
I have an STM32L011 on a board I am developing.I can enter the bootloader no problem, as per AN2606/AN3155. I am using USART2, 57600 baud.I can program FLASH/erase FLASH/read FLASH - all works as expected.I note that the bootloader reserves 2048byte...
I am working with a dual core STM32H755 and attempting to create a shared memory location for the two cores to access. I am attempting to do this by modifying the linker script. I have added the following lines to the M7 core linker script, in the S...
用SPI+DMA驱动AD4001,用片选信号代替 CONV,采集一个正弦信号。Normalnormal正常,循环模式却不对,求大佬解答!!Normal模式下,每次在 HAL_SPI_RxCpltCallback 函数里面重新启动数据正常,能看到正弦变化规律 循环模式下数据就不对了,采集的同样一个交流信号,我在半传输完成回调里面查看,按道理后半部分的数据应该是正常的正弦变化才对,实际却不是,但是去采集直流时又是正常的。 ...
Hello Tesla I need to run M4 from 0x08000000 and then M7 from 0x08100000. Is there any example ? Exactly I v'done my BOOT that runs on M4 (0x08000000) loads the Flash , then jumps into M4 (0x08040000). Now i have to run M7 from 0x08100000, but i d...
/** * @brief DMA Linked-list yWaveQ configuration * @PAram None * @retval None */ HAL_StatusTypeDef MX_yWaveQ_Config(void) { HAL_StatusTypeDef ret = HAL_OK; /* DMA node configuration declaration */ DMA_NodeConfTypeDef pNodeConfig; ...
I am trying to implement a GPDMA driver in a C project that does not use HAL, and have been really struggling to get something working. I have read everything I can find on this peripheral, multiple times, and still don't quite understand how one wou...
I am trying to debug some functions to write to the memory mapped QSPI. When I go to debug it, I notice that before any functions even run the QPSI is in HAL_QSPI_STATE_ERROR, therefore I cannot test my code to see if is running because it is depende...
Are the steps followed for RTC calibration the same for crystal and temperature variation?How is the calibration register value selected for temperature variation?
I have selected the RTC calibration as 512Hz. Will I be able to perform RTC smooth calibration if my frequency obtained on the RTC calib pin is beyond the range 511.75Hz - 512.25Hz. How do I calibrate the RTC beyond this range ??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.