2025-05-07 3:11 AM
Hello, I am working with an STM32G4 microcontroller and noticed an unexpected behavior regarding Bit 20 (BFB2) in the User & Read Protection Option Bytes.
According to the reference manual, BFB2 is a read-only bit.
After performing an option bytes erase in Keil, I expected BFB2 to be cleared to 0 (default).
However, after a system reset, I observed that BFB2 is set to 1.
I would like to understand:
Who sets BFB2 to 1 after an option bytes erase?
Is this controlled by bootloader behavior, internal flash controller logic, or some default hardware mechanism?
2025-05-07 5:42 AM
If you want BFB2=0, perhaps set it explicitly. There is no "option byte erase" procedure at the mcu level, so this is something Keil-specific being done.
2025-05-07 6:05 AM
In Reference Manual RM0440, the User & Read Protection Option Bytes are documented at Flash memory address 0x1FFF7800 with an ST production value of 0xFFEF F8AA. However, when I print the User & Read Protection Option Bytes, I get 0xFFFF F8AA, which does not match the documented production value.
I expected Bit 20 (BFB2) to be 0 (the default ST production value) because I had deleted the option bytes using Keil. I want to understand who sets BFB2 to 1, even though User & Read Protection Option Bytes are read-only.
I don’t necessarily want BFB2 to be 0, but initially, after deleting the option bytes, I checked and BFB2 was 0. Once the option bytes were properly set after the initial factory configuration, they were never configured again. However, now I can’t use that same logic to configure the option bytes.
2025-05-07 6:37 AM - edited 2025-05-07 6:38 AM
Keil is setting those bytes. They do not change arbitrarily.
You can use STM32CubeProgrammer to set them if you'd like.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.