STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

system header deterioration bug ...

I recently struggled with the SPI peripheral of the stm32c031, the reference manual is somewhat veiled on occasions.Anyway, taking a closer look at the relevant system header part, I saw this : * @file stm32c031xx.h * @author MCD Application T...

_legacyfs_online_stmicro_images_0693W00000blENLQA2.png
Ozone by Principal III
  • 3220 Views
  • 4 replies
  • 0 kudos

Cleaning after reflow: STM32L151VC6 UFBGA100 package

Hallo, I have a question for the STM32L151 in the UFGBA100 package.There is a technical note  for the WLCSP-package existing (TN1163). In this note it is not recommended to clean the WLCSP package and also apply no ultrasonic cleaning methods.We are ...

geigerm by Associate
  • 1044 Views
  • 0 replies
  • 0 kudos

Failed to get BIC code for P-L496G-CELL02 ESIM activation

I follow the instructions on "How to enable SIM MFF2 connectivity with P-L496G-CELL02.txt" from the link of "https://www.st.com/en/evaluation-tools/p-l496g-cell02.html#tools-software" utilities section.The device was configured and actived ESIM, afte...

XYang.3 by Associate II
  • 1247 Views
  • 0 replies
  • 0 kudos

CAN Rx FIFO Mail Boxes

HelloI have a query regarding mailboxes for receiving FIFO in CAN peripheral. The manual says there are two FIFOs and each FIFO has three mailboxes. So, it means there should be total SIX registers for receiving DATA. But I see only two registers CAN...

Nico3 by Senior
  • 1243 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F103C6T6 Flash Size is incorrect reporting 32 and not 64

stm32cubeprogrammer v2.13.0 reporting incorrect sizeAs is st-infoFound 1 stlink programmersversion: V2J41S7serial: 6600240013000039544B524Eflash: 32768 (pagesize: 1024)sram: 10240chipid: 0x0412descr: F1 Low-density deviceI am on ubuntu 23.04Any help ...

bibble235_0-1687093691011.png
bibble235 by Associate III
  • 1953 Views
  • 2 replies
  • 1 kudos

SAI DMA circular mode

I'm working on the SAI part to read the ICS4342MIC through I2S protocol, and looking for a way to stream a large amount of data from the microphone to the hyper ram (in memory mapped mode). The current available feature of the HAL_SAI_Receive_DMA fun...

VPHAM.1 by Associate
  • 1970 Views
  • 2 replies
  • 1 kudos

STM32WL55 - ADC conversion time

Hello everyone!I'm working on STM32WL55JCI7 board and trying to run ADC at the fastest speed (min total conversion time mention on datasheet 0.4uSec) and I don't receive this time.My configuration is the following:And to measure total time of convers...

MichaelMor_0-1687075081305.png MichaelMor_1-1687075306648.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.