2023-06-18 9:15 PM
I follow the instructions on "How to enable SIM MFF2 connectivity with P-L496G-CELL02.txt" from the link of "https://www.st.com/en/evaluation-tools/p-l496g-cell02.html#tools-software" utilities section.
The device was configured and actived ESIM, after that, tried to get BIC code, however, got negative response, as shown in the following:
I tried 2 P-L496G-CELL02, both gave the same results. Please help...
1. Type In "at at<CR>", got the expected response:
ATParser:*** SEND (size=3) ***
at<CR>
<CR><LF>
OK<CR><LF>
2, type in "at ati<CR>"
ATParser:*** SEND (size=4) ***
ati<CR>
<CR><LF>
Quectel<CR><LF>
BG96<CR><LF>
Revision: BG96MAR02A08M1G<CR><LF>
<CR><LF>
OK<CR><LF>
3. Type In "at AT+CRSM=176,12275,0,0,16,,"3F00"<CR>", however, got negative response.
ATParser:*** SEND (size=33) ***
AT+CRSM=176,12275,0,0,16,,"3F00"<CR>
<CR><LF>
+CME ERROR: unknown<CR><LF>
ATCore ERROR:AT_sendcmd error
ATCore ERROR:AT_sendcmd error: parse from rsp
LOG ERROR #1: channel=2 / errorId=11 / gravity=2
LOG ERROR #2: channel=2 / errorId=14 / gravity=2
CS ERROR:<Cellular_Service> error when sending direct cmd
AT+CRSM=176,12275,0,0,16,,"3F00" command FAIL
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.