STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debugging STM32f405 using Nucleo board .

Hello Team,I debug STM32F405 on my custom PCB using nucleo board and STLink utility software.Now, I have added a digital isolator on my PCB , and the STM32F405 MCU is powered by the isolated  3.3v supply & ground  of the isolator.Now, the Nucleo boar...

SMour.2 by Associate III
  • 2975 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with UART communication functions.

All these functions have one problem, let's say in this function HAL_UART_Receive_IT(&huart4, data,5);the third parameter is the number of transmitted characters.If you enter more or less characters in the COM port of the terminal than specified in t...

MMust.5 by Senior II
  • 2882 Views
  • 2 replies
  • 0 kudos

Can HAL_CAN_AddTxMessage Not Transmit.

Hi I try to send a message to the CAN interface, use HAl functionHAL_CAN_AddTxMessage.But the message not send.I verify with debug that the interface is allwais in Listering HAL_CAN_STATE_LISTENING.Do you have idea what is wrong?uint8_t CAN_TX(int16_...

PZamb.2 by Associate III
  • 2051 Views
  • 1 replies
  • 0 kudos

UART information missing from RefMan, HAL_UART_Init() error

I found this problem with STM32L476 but I suspect it may be a general STM32 quirk.The manual does not list the minimum and maximum value of UART BRR register. While the minimum value of 0x10 seems to be quite obvious, the maximum correct value in the...

gbm by Principal
  • 1785 Views
  • 0 replies
  • 2 kudos

Help finding example projects

Hello everyone, I’m currently trying to use an stm32l4r9i discovery along with a b-cams-omv. I saw that this camera is listed as a supported product for this board, however, I cannot find an example project of these working together. If anyone knows ...

DLowry by Associate
  • 2566 Views
  • 3 replies
  • 1 kudos

H7 series FMC question

Hi, I am using STM32H725 with the FMC interface and trying to clarify some issues.The initial issue was seeing extra writes/reads on the bus - this seemed to be fixed by switching the banks to use the 0xC...0 address range or configuring the original...

OHaza.1 by Associate III
  • 2341 Views
  • 2 replies
  • 0 kudos

Resolved! Why won't my DAC output a voltage larger than 2.56v?

Hi there,I've been having difficulty trying to make the DAC channel 1 output 3.3v. The largest voltage that the DAC outputs is 2.56 volts which I measured with an oscilloscope. I try to set the output voltage to be higher with the following code snip...

RWang.9 by Associate II
  • 9085 Views
  • 16 replies
  • 1 kudos

STM32H7 I2S no data on Data line

Hello, I am interfacing audio Codec SGTL5000 with STM32H7 Nucleo board. I2S peripheral is initialized using the HAL init function. I converted a wav file to a C array and trying to transmit that to the Codec. STM32 is configured as Master TX and Code...

panrod by Associate II
  • 4751 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.