STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Internet application STM32F407 + DP83848

Hi all, I develop a network application for EVSE. I would like to ask question related to MAC address. is it possible change the MAC address of DP8348? As I need to use DP83848 for websocket application.Is there any method to store data in STM32f4?Th...

ISM330DHCx Angle Reading Error

Hi , STM Community i was using the ISM330DHCx 3D accelerometer and gyroscope Sensor for Angle Measurement purpose.And decided to try with MOTION_FX libraryA  because i found an example related to this library.i was able to get the Accelerometer and g...

3-wire SPI (SSC) configuration

HiI want to read out a sensor, which has an SSC interface, as depicted in the image attached. The IC is a TLE5012B (https://www.infineon.com/dgdl/Infineon-Angle_Sensor_TLE5012B-UM-v01_02-en-UM-v01_02-EN.pdf?fileId=5546d46146d18cb40146ec2eeae4633b) an...

HL?�t by Associate II
  • 8595 Views
  • 7 replies
  • 0 kudos

I want to use an expansion MEM board

I want to use an expansion MEM board and I followed this article: https://stcommunity.st.com/t5/stm32-mcus/how-to-install-and-import-an-x-cube-expansion-package-with/ta-p/49853 .The problem is when I generated the code and tried to build the project,...

Screenshot_5.png Screenshot_6.png
JSanc.7 by Associate II
  • 908 Views
  • 0 replies
  • 0 kudos

How to re-fetch the RTC value after power restored

Hi allI working on the RTC on the STM32U585 with battery backup, after the date/time been set and running i want to re-fetch these values once the device restores the main power or happens even after reset (with main power), As i have a batterybackup...

meghasb by Senior
  • 993 Views
  • 1 replies
  • 1 kudos

What is the conversion time for a single ADC channel

I’m using  STM32L433RCT6TR, the ADC conversion time mentioned is 0.185uS to 8.1625uS in the data sheet. Is this the time taken by individual ADC channel or the entire 16 ADC channels. What will be the maximum input signal frequency which I can give i...

Examples in STMCUBE IDE 1.12.1

This my first time here and using STM32 MCUs.I am wondering how locate the examples in this STMCUBE IDE version,I would need them for Nucleo L063RZThanks.

AMV by Associate
  • 2084 Views
  • 3 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.