Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello guys, I would like to know if it is possible to directly connect NUCLEO-F446RE board with steval-mic003v1 mic array without any expansion board. Would love to know your feedback and much appreciated.
New question moved from this post. Another question: which is the best way to proceed for the schematic design of a custom board with series G49 or H5? is it better to: - start from the datasheet of the MCU, - or from some applications notes like thi...
I'm using a * STM32N6-DK * Brightsense VD56G3 I've made 2 camera drivers so far and the only difference i can see from the cameras is that my first camera module has MIPI short packets start and stop. I'm making this observation from the scope. So...
Dear STMicroelectronics Support Team, I am working with two ST-LINK/V2 debuggers and have observed a difference in the VTref (VAPP) signal location on the 20-pin connector. I would like to understand whether this is expected behavior. Details of ...
Hello all, I want to connect a 3.3 V I2C based keypad with STM32U5G9J-DK1 via a carrier board on which the STM32 board sits via expansion connectors CN9 and CN10 present on it. I am using pins PG13, PG14, and PG9 for my I2C SDA, I2C SCL, and INTERRUP...
Dear people, I use these little square pins and headers (see image), to obtain access to the contacts of CN11 / CN12 of Nucleo Boards, e.g. H723ZG, or F756ZG?. However these are impractical, because movement or vibration might lead to interruptions...
Dear all,I'm unable to connect via SWD to my STM32F103C8T6. What ever I try I get no target found with STM32CubeProgrammer or ST-LINK Utility (I have tried all combinations at slow and high speeds). - device is virgin- BOOT0 is low- NRST unconnected ...
Hello everyone, I’m facing an issue while trying to debug my project custom_for_stm32f103c8t6 in STM32CubeIDE. When I launch the debug session, I get the following error message: Error in final launch sequence:Failed to start GDB server What I’ve t...
Hi, I tried to configure the USB Host for a project, but it’s difficult to configure, and I am not finding any online support available for the STM32H5 series controller.My requirement: I configured PB4 as an output, which is connected to a green LED...
I have a NUCLEO-F103RB (MB1136 rev C05). My goal is to remove the ST-LINK and power via a hat supplying 3.3v. For the 3.3v I have: Moved JP5 to pins 2-3.Checked JP1 is removed.Removed SB2 zero ohm resistor.Removed SB12 zero ohm resistor.Verified my s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.