Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi all,I am designing a custom PCB using the STM32N657Z0 and am looking for some advice on how to treat some of the specialized pins that I don't plan on using. Specifically I have not been able to find any recommendations on how to treat any of the ...
Is there a detailed user manual available for the NUCLEO-U3C5ZI-Q?The product page links to a generic getting started document and a generic document on Nucleo 144 boards, but I can't see anything that lists the I/O or that documents the links.
Hello!I was working on a project of mine and put it on pause for a few weeks and now when I tried to connect the stlink to my PC its no longer detected. Its not showing up in the device manager and the stlink has dim red and green lights lit.Does thi...
Hello everyone! I'm new to the NUCLEO-H743ZI2 board. I need help with two questions: 1) I can't find a description of the STLK backup port -CN2 anywhere. Can you tell me if I can use it to program other STM32 devices on other boards, and how? 2) C...
Hello,I am currently experiencing some difficulties using the NUCLEO-N657X0-Q board.I am using STLinkUpgrade v3.17.10, and the device ID is correctly recognized as 003500244142501120353451, as shown in the attached image.However, when I click "Open i...
Hi,for a project involving a custom educational flight controller, I need to use the following hardware:- steval-FCU001V2 board- steval-drone02 drone kitFor clarity, here are st product page links that i used.Manual:https://www.st.com/resource/en/use...
Hi,I'm using STM32H755 Nucleo board and I'm evaluating ADC. I'm using 1.92MSPS per ADC sample rate for ADC1 and ADC2. I'm using A0 and A5 pins from CN9. I'm using ethernet to transfer data. My input to A0 (I channel) is 100kHz sine and A5 (Q channel)...
Trying to flash F1 and F0 series boards (not a clone, resoldered the MCU with a genuine from mouser) with L4 ST link V2.1, but having no success. Doing the basic CN2 headers out, CN3 VDD(with or without), SWCLK, GND, SWDIO. Spamming every option in ...
I’m using the X-NUCLEO-LPM01A (PowerShield) and previously had firmware version 1.0.1, where I could connect via a serial terminal over USB and interact with the board using commands. But error occured short after, with LED 2 on the board indicating ...
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.