Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I’m having a problem with a board I’m developing based on the STM32H747BIT6. The issue is related to SPI communication. When I connect any device to the SPI bus, the signal level drops from 3.3 V to around 1.5 V. I have tested different SPI pe...
Hi all, I have a small issue with the STM32N6570-DK board and the VENC_SDCard example code. The PN12 pin has a voltage of 0V (card inserted) or 1.80V (no card inserted); on the MCU side, the GPION data register (IDR) always shows a logic 0 in both si...
Hello ST Community,My name is Gorakhnath. I am currently pursuing M.Tech (Power Electronics and Drives) at NIT Kurukshetra. I am using the STM32F4DISCOVERY (STM32F407VGT) board and I need stable DAC outputs for my hardware application.What I need (re...
Hello,I got a radio MCU which connects to cloud and can receive binaries from database. And I got a STM32 that controls some stuff, including other MCUs. In production this means a lot of headers and programming time for all of them, no way to update...
Hi, I’m using a NUCLEO-144 (STM32H563ZIT6) development board with only the board USB STLINK-V3EC port connected. TRACE and DEBUG are enabled with Serial Wire in the configuration file, and printf is routed through ITM: int _write(int file, char *ptr,...
When will the NUCLEO-C5A3ZG be available via distributors?The st.com site lists it as available(mass production), but none of the distributors has listed it at all. And the estore lists it as coming soon. Do you have any more concrete dates, will it...
Hi ,Recently I got a NUCLEO-C051C8 board and tried to connect it to windows and program it using STm32CubeIDE but it does not show that st-link is connected , ST-link on board blinks RED continuously. Cant install it ( installation goes through , but...
Hi For some of my project, I need to measure the power consumption of the STM32N6570-DK while running a model on the CPU only versus an NPU + CPU accelerated workload. I am following the guide 1. How to measure power on the STM32N6 - STMicroele...
Hello All,I have the NUCLEO-C562RE board and I wanted to get started with it. But I am lost and not able to find any documentation related to architecture manual or user manual. I am new to ST boards, previously I used Aurix TC375. Has someone here i...
I have the following original debuggers:Stlink V2Stlink V3_SETStlink V3_MINIE (2 pieces)I was recently testing a simple board with an STM32U083 (powered by 3.3V) and found that two Stlink V3 MINIE units could connect to the MCU. Meanwhile, both the V...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.