2019-03-05 2:01 PM
When I try to set up quad SPI with dual bank on an STM32H7, I get the following message:
"You must select a ChipSelect signal for Dual bank mode first"
This is true even for a blank project with nothing else assigned. I don't see anywhere available to select the chip select lines.
Solved! Go to Solution.
2019-03-05 10:50 PM
Hello @Adrian Adamson
Thanks for the feedback.
You are right, This issue will be fixed in the next CubeMX release.
Best Regards,
Khouloud.
2019-03-05 10:50 PM
Hello @Adrian Adamson
Thanks for the feedback.
You are right, This issue will be fixed in the next CubeMX release.
Best Regards,
Khouloud.
2019-03-06 9:58 AM
Thank you for your help. Hopefully the update will be soon. I'm working on the board layout now and I do need to know which pins to route to for those chip selects. I guess for now I should assume that they are the same pins used for NSS in the other QSPI modes?
2019-03-06 1:29 PM
Will PM you schematic section I've worked from.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.