2019-03-05 5:59 AM
Hi
I am using STM32Cube V1.0 , version 4.24.0 along with Atollic TrueSTUDIO® for STM32 V9.0. Within Cube I created the project with USB, and created the source code. When I try and compile it I get a bunch of HAL errors, HAL_init() undefined and a bunch of HAL_RCC... commands undefined. I havent done anything different as I have done than creating other projects , straight forward. The .h files seem to be there. Has anyone else have this issue, or know what I have done wrong?
Thanks
Scott
Solved! Go to Solution.
2019-03-06 12:54 AM
Hello @Scott Dev ,
Please upgrade to latest STM32CubeMX V5.1.0 release and STM32CubeL4 V1.13.0, then tell us if you are facing same issue
Kind Regards,
Imen
2019-03-06 12:54 AM
Hello @Scott Dev ,
Please upgrade to latest STM32CubeMX V5.1.0 release and STM32CubeL4 V1.13.0, then tell us if you are facing same issue
Kind Regards,
Imen
2019-03-07 4:04 AM
Hi Imen
Version 5.1 seemed to work, many thanks. What is STM32CubeL4? I havent used that before.
Thanks
Scott
2019-03-07 4:57 AM - edited 2023-11-20 9:34 AM
Hi @scott Dev ,
You are using STM32CubeMX with the STM32CubeL4 firmware package, which can be downloaded through STM32CubeMX following the steps below:
Select Help > Manage embedded software packages to open the Embedded Software Packages
The procedure is described in UM1718, Section 3.5.2: Installing STM32 MCU packages.
You can check the"Project Manager" view in your STM32CubeMX project to see the firmware package version used:
Kind Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.