cancel
Showing results for 
Search instead for 
Did you mean: 

[BUG] CAN init code using CUBEMX

jd kim
Associate II

Hi, Im using stm32f1 serise and today updated my cube mx

so now version is 5.0.1

I just found that can init code is several changed,

but it's some kind simple missing error

in main,

static void MX_CAN_Init(void)
{
 
  /* USER CODE BEGIN CAN_Init 0 */
 
  /* USER CODE END CAN_Init 0 */
 
  /* USER CODE BEGIN CAN_Init 1 */
 
  /* USER CODE END CAN_Init 1 */
  hcan.Instance = CAN1;
  hcan.Init.Prescaler = 3;
  hcan.Init.Mode = CAN_MODE_NORMAL;
  hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
  hcan.Init.TimeSeg1 = CAN_BS1_8TQ;
  hcan.Init.TimeSeg2 = CAN_BS2_3TQ;
  hcan.Init.TimeTriggeredMode = DISABLE;
  hcan.Init.AutoBusOff = DISABLE;
  hcan.Init.AutoWakeUp = DISABLE;
  hcan.Init.AutoRetransmission = DISABLE;
  hcan.Init.ReceiveFifoLocked = DISABLE;
  hcan.Init.TransmitFifoPriority = DISABLE;
  if (HAL_CAN_Init(&hcan) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN CAN_Init 2 */
 
  /* USER CODE END CAN_Init 2 */
 
}

but in stm32f1xx_hal_can.h,

typedef struct
{
  uint32_t Prescaler;  /*!< Specifies the length of a time quantum.
                            This parameter must be a number between Min_Data = 1 and Max_Data = 1024 */
 
  uint32_t Mode;       /*!< Specifies the CAN operating mode.
                            This parameter can be a value of @ref CAN_operating_mode */
 
  uint32_t SJW;        /*!< Specifies the maximum number of time quanta
                            the CAN hardware is allowed to lengthen or
                            shorten a bit to perform resynchronization.
                            This parameter can be a value of @ref CAN_synchronisation_jump_width */
 
  uint32_t BS1;        /*!< Specifies the number of time quanta in Bit Segment 1.
                            This parameter can be a value of @ref CAN_time_quantum_in_bit_segment_1 */
 
  uint32_t BS2;        /*!< Specifies the number of time quanta in Bit Segment 2.
                            This parameter can be a value of @ref CAN_time_quantum_in_bit_segment_2 */
 
  uint32_t TTCM;       /*!< Enable or disable the time triggered communication mode.
                            This parameter can be set to ENABLE or DISABLE. */
 
  uint32_t ABOM;       /*!< Enable or disable the automatic bus-off management.
                            This parameter can be set to ENABLE or DISABLE */
 
  uint32_t AWUM;       /*!< Enable or disable the automatic wake-up mode.
                            This parameter can be set to ENABLE or DISABLE */
 
  uint32_t NART;       /*!< Enable or disable the non-automatic retransmission mode.
                            This parameter can be set to ENABLE or DISABLE */
 
  uint32_t RFLM;       /*!< Enable or disable the receive FIFO Locked mode.
                            This parameter can be set to ENABLE or DISABLE */
 
  uint32_t TXFP;       /*!< Enable or disable the transmit FIFO priority.
                            This parameter can be set to ENABLE or DISABLE */
}CAN_InitTypeDef;

could you guys fix it ASAP?

thanks with regards

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @jd kim​ ,

Can you please share your ioc file?

Which firmware package CubeF1 are you using ?

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hello @jd kim​ ,

Please ensure to use the latest STM32CubeF1 firmware package (V1.7.1) with latest version of STM32CubeMX (V 5.1.0).

After check with these latest versions, we aren't able to reproduce your issue and the CAN generation code and structure definition are correct.

Here is the stm32f1xx_hal_can.h:

/**
  * @brief  CAN init structure definition
  */
typedef struct
{
  uint32_t Prescaler;                  /*!< Specifies the length of a time quantum.
                                            This parameter must be a number between Min_Data = 1 and Max_Data = 1024. */
 
  uint32_t Mode;                       /*!< Specifies the CAN operating mode.
                                            This parameter can be a value of @ref CAN_operating_mode */
 
  uint32_t SyncJumpWidth;              /*!< Specifies the maximum number of time quanta the CAN hardware
                                            is allowed to lengthen or shorten a bit to perform resynchronization.
                                            This parameter can be a value of @ref CAN_synchronisation_jump_width */
 
  uint32_t TimeSeg1;                   /*!< Specifies the number of time quanta in Bit Segment 1.
                                            This parameter can be a value of @ref CAN_time_quantum_in_bit_segment_1 */
 
  uint32_t TimeSeg2;                   /*!< Specifies the number of time quanta in Bit Segment 2.
                                            This parameter can be a value of @ref CAN_time_quantum_in_bit_segment_2 */
 
  FunctionalState TimeTriggeredMode;   /*!< Enable or disable the time triggered communication mode.
                                            This parameter can be set to ENABLE or DISABLE. */
 
  FunctionalState AutoBusOff;          /*!< Enable or disable the automatic bus-off management.
                                            This parameter can be set to ENABLE or DISABLE. */
 
  FunctionalState AutoWakeUp;          /*!< Enable or disable the automatic wake-up mode.
                                            This parameter can be set to ENABLE or DISABLE. */
 
  FunctionalState AutoRetransmission;  /*!< Enable or disable the non-automatic retransmission mode.
                                            This parameter can be set to ENABLE or DISABLE. */
 
  FunctionalState ReceiveFifoLocked;   /*!< Enable or disable the Receive FIFO Locked mode.
                                            This parameter can be set to ENABLE or DISABLE. */
 
  FunctionalState TransmitFifoPriority;/*!< Enable or disable the transmit FIFO priority.
                                            This parameter can be set to ENABLE or DISABLE. */
 
} CAN_InitTypeDef;

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.