STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMx discrepancy with Reference Manual for the STM32F767NIx DMA

Hello,I am working on a project for a STM32F767NIHx. I am using the STM32CubeMx tool and validating using RM0410. The problem I am having is that the i2c4_tx peripheral is not listed in dma1 stream5 on page 248 of the reference manual. CubeMx, howeve...

R_1 by Associate III
  • 1571 Views
  • 2 replies
  • 1 kudos

Release build not defining compiler

Posted on March 29, 2018 at 22:22I am using the latest TrueStudio with a project for STM32L452 created using the latest STM32CubeMX.The created project contains both a debug and a release build. When I set the debug as active and look in one of the ...

Resolved! STM32L4 USB VCP project not compiling

Hi I am using STM32Cube V1.0 , version 4.24.0 along with Atollic TrueSTUDIO® for STM32 V9.0. Within Cube I created the project with USB, and created the source code. When I try and compile it I get a bunch of HAL errors, HAL_init() undefined and a ...

Resolved! Error setting up dual bank quad SPI

When I try to set up quad SPI with dual bank on an STM32H7, I get the following message: "You must select a ChipSelect signal for Dual bank mode first"This is true even for a blank project with nothing else assigned. I don't see anywhere available...

[BUG] CAN init code using CUBEMX

Hi, Im using stm32f1 serise and today updated my cube mx so now version is 5.0.1I just found that can init code is several changed,but it's some kind simple missing errorin main, static void MX_CAN_Init(void) {   /* USER CODE BEGIN CAN_Init 0 */  ...

jd kim by Associate II
  • 1327 Views
  • 2 replies
  • 0 kudos

USART LL creation problem

HelloI m using STM32CubeMX 5.1.0 with STM32CubeF1 Firmware V1.7.0 09-October-2018I try to generate the LL for use USART1 and USART2 over STM32F103RCT6, when the Cube generated the code I have the follow problems LL_USART_InitTypeDef (undeclared ident...

Bug in STM32CubeMX v5.1.0 with STM32F103CBT6 + FreeRTOS

My project work fine with STM32CubeMX v5.0.1.I upgraded to v5.1.0, It generated code miss something.My project detail: stm32f103cbt6 + freertos,SYS -> Timebase Source: TIM1-----Generated code stm32f1xx_it.c missing a line: HAL_TIM_IRQHandler(&htim1);...

BD8NCF by Associate
  • 1283 Views
  • 2 replies
  • 0 kudos

Bonjour, Comment puis-je établir une communication entre deux cartes stm32f411? je remerci tout aide. Merci beaucoup.

J'ai un projet qui consiste à comuniquer deux cartes stm32f411, j'ai essayé de le faire par connexion "usart", mais je ne suis pas arrivé encore à les communiquer, j'utilise les fonctions Hal, pour la transmission et la réception, elles fonctionnent ...

lmeli by Associate II
  • 1767 Views
  • 2 replies
  • 0 kudos

Setting up USB storage with HAL/CubeMX

Hello:I have used CubeMX to generate base code for a USB storage device in host mode. The last I see of it in the code is the call in main: "MX_USB_OTG_FS_HCD_Init();"Now I would like to take the next big step and try to connect, and write/read. Is t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.