STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 6.16.0 released

We are pleased to announce that STM32CubeMX 6.16.0 release is available. What is new in 6.16.0: Added support for new microcontrollers across the STM32WBA, STM32N6 and STM32H5 series and the STM32WL3x product line. The related new boards include the...

Aimen1 by ST Employee
  • 2907 Views
  • 5 replies
  • 7 kudos

Resolved! Update Eclipse IDE

Hey, I want to open a project from my peer, but i cant because the version for STMCubeMX with which it was generated is newer then mineI then do that and 'Check for Updates', which doesn't work and gives me an error. When i try to manually access the...

adriananthony066_0-1761760947038.png adriananthony066_1-1761761078916.png

Resolved! About TouchGFX frame buffer problem

Hello, I'm using TouchGFX on an STM32L452RET6 with an SPI screen. The screen has integrated GRAM, so I selected the partial buffer option in STM32CubeMX. STM32CubeMX generated the partial buffer code as expected, but it also generated code for a full...

PixPin_2025-11-05_13-41-38.png PixPin_2025-11-05_13-43-10.png
TomBrown by Associate
  • 712 Views
  • 3 replies
  • 0 kudos

Resolved! USB STM32G0B1KCT6 not working

Hi I have used STMCubeIDE 1.11.0 (Cube 1.6.1) to generate the code for USB CDC interface for STM32G0B1.The code is as CubeMX would generate. I have not modified the code at all.When I plug the device into a PC I get "USB device not recognized" I have...

DCorn by Associate III
  • 9264 Views
  • 10 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.