STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Problems related with NetXDuo

Hello everyone,I'd like to report some issues I encountered while using NetXDuo to create a UDP server with a Nucleo-N657X0-Q board:There's no option to select a network interface other than the custom one — I had to manually add all the libraries re...

LisaB by Associate III
  • 2918 Views
  • 8 replies
  • 2 kudos

GPIOS for CSI on stm32n6

Hello,while configuring the CSI interface for camera , on its enablement in the STM32CubeMX why I can’t see the GPIOs corresponding to it in the flip section? does it has any dependency on any other peripheral?or clock setting?under the configuration...

darla14 by Senior
  • 1633 Views
  • 7 replies
  • 0 kudos

Resolved! CubeMX 6.15 does not regenerate code

Hi all,I recently updated the IDE to v1.19 and MX to v6.15.0, and the MX code generation is no longer working for me.After some testing, I found out I can create new projects and code is (apparently) well generated. After this first generation, if i ...

ACC_1-1763046480260.png
ACC by Associate II
  • 792 Views
  • 4 replies
  • 1 kudos

Resolved! STM32F107+Ethernet+Lwip no longer an option?

STM32CubeIDE Version 1.19.0Build: 25607_20250703_0907I created a project using the STM32F107 and Ethernet. Everything was setup using the .ioc template with Ethernet and various GPIO stuff. Lwip was not included. I generated the code and all of the E...

Starting a new project from a board NUCLEO-F767Zi

Hi,Using STM32CubeMX version 6.15.0When I start a new project from the NUCLDO-F767ZI board I just get a blank chip, none of the component configuration at all, I tried it on two PC's both the same.This used to work and was quite handy starting a new ...

RickHamilton_0-1762946697548.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.