STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! Why no Synchronous Trace option for STM32G474RE in CubeMX?

Hi,I am trying to set Debug under Sys to "Synch Trace" in latest CubeMX but there is no such option for my STM32G474RE: On other screenshots on the internet I see those options: Any idea why?Is Synch Trace not available on the 64 pin package???Thanks...

0693W000007DtxqQAC.jpg 0693W000007DtyjQAC.jpg
Anguel by Senior
  • 1256 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H723 Pinout PC2_C/PC3_C

Hello everybody!The documentation indicates that this leg can only be configured as an ADC input. In "CUBE MX" it can be defined as different kinds of interfaces. Who should I believe that my project would work properly and I would not be faced with ...

0693W000007BWxFQAW.png 0693W000007BWxKQAW.png 0693W000007BWxPQAW.png
AB.19 by Associate II
  • 2834 Views
  • 2 replies
  • 0 kudos

Resolved! Can't create MDK-ARM project for STM32L011F4U

Cube version: 6.1.1Java: Oracle SE 15.0.2 (64bit)Toolchain: MDK-ARM V5Part: STM32L011F4UWhen I create an empty project and press generate, the generation fails. First I get a empty dialog screen:And then an error:Is this a bug?

0693W000007Du3eQAC.png 0693W000007Du4NQAS.png
allard by Senior
  • 1283 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE bug or not?

I use STM32CubeIDE under MacOS. I don't understand whether it is a bug or not. I can not change Input frequency of HSE in clock configuration. I can do it in CubeMX under Window on the same project.

0693W000007DJGlQAO.png
EL314 by Associate III
  • 1556 Views
  • 2 replies
  • 0 kudos

Enabling Ethernet Interface on Nucleo-H743ZI2

Hi,I am developing a TCP/IP server for my application on the Nucleo-H743ZI2 board. I want to use LWIP with FreeRTOS to allow threading and have a similar syntax to POSIX sockets.So far I found the following two examples:(1) This tutorial targets the ...

0693W000007CsFWQA0.png 0693W000007CsJJQA0.png 0693W000007CsIWQA0.png 0693W000007CsJxQAK.png
HA87 by Associate III
  • 8707 Views
  • 8 replies
  • 1 kudos

Resolved! MII on STM32H730VBTx

STM32CubeMX doesn't show MII as an option for Ethernet on the STM32H730VBTx. Is MII not available on this part (RMII only?) or is there a problem with STM32CubeMX? The datasheet suggests it should support MII.

Aasdf.3 by Associate
  • 1655 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.