STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! I can't find the PULL UP menu in STM32CubeMx. (to use i2c1)

Hi AllI have simple question about STM32CubMX.I use the STM32F103RBT and test the i2c with eeprom.When I set the pin for i2c, I should change the GPIO Pull-up/Pull-down in STM32FCubMx.But This menu is not in STM32FCubMX.I don't connect external pull ...

0693W000007ERMPQA4.png
dKim.1 by Associate II
  • 4131 Views
  • 2 replies
  • 0 kudos

Are STM32F7Cube code examples configured with CubeMX ?

Hi, The SDK package provided in STM32F7Cube has many code examples on all topics but is that code initialized with CubeMX ? Or, otherwise , if it is not , in order to reconfigure or customize it the user has to manually merge that code with the one ...

eBirdman by Senior II
  • 1466 Views
  • 2 replies
  • 0 kudos

H7 LL EXTI 1.8.0 fails to enable interrupt, but works with HAL

Using STM32CubeIDE 1.5.1, H7 firmware library 1.8.0, NUCLEO-H743ZI:The blue "User" button is tied to PC13. Using the HAL library, I am able to generate an interrupt when the button is pressed (rising edge).When I change the GPIO to use the LL librar...

dale by Associate III
  • 906 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.