STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! stm32cubef3 v1.11 build error in IAR IDE

I compiled the stemwin example of stm32cubef3 v1.11.0 with IAR v9.10. If the optimizations of the c/c++ compiler is high (size), there is no problem, but if it is None or Low, the following error occurs. stm32f3xx_hal_rcc.c   Tool Internal Error:   I...

Iyoon.1 by Associate II
  • 3878 Views
  • 7 replies
  • 0 kudos

Resolved! Nx_Iperf example code fails to install

I use STM32MxCube to install example code. I selected STM32H7 to finde the Nx_Iperf example for the STM32H747I-DISCO board. When I select Start Project, the progress bar runs to completion then I get a message "FAILED TO INSTALL EXAMPLE: Nx_Iperf"....

EBerl.1 by Associate II
  • 1576 Views
  • 2 replies
  • 0 kudos

Is it possible to make friends HAL_TIM_PWM_Start_DMA (& htim1, TIM_CHANNEL_3, (uint32_t *) Buff, counter); with Repetition Counter.

I tried on STM32F103C8Tx. The timer simply swallows the "repetition counter" of the DMA values ​​on the next update.I was asked to make a simple example of playing a short wav file at a bit rate of 88 Kbps to attract the operator's attention.The abov...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.