2021-04-15 12:33 AM
I compiled the stemwin example of stm32cubef3 v1.11.0 with IAR v9.10. If the optimizations of the c/c++ compiler is high (size), there is no problem, but if it is None or Low, the following error occurs.
stm32f3xx_hal_rcc.c
Tool Internal Error:
Internal Error: [AsmLine - OgAsm]: Error: Invalid shift amount LSRS R6,R6,#+0
Internal Error: [AsmLine - OgAsm]: Error: Invalid shift amount LSRS R6,R6,#+0
How do I fix the error?
Solved! Go to Solution.
2021-04-27 9:32 AM
It's their error message - so they would be the best placed to understand what, exactly, would cause it to say that.
And you say there is no error when using an earlier IAR version - so you should at least be asking IAR what they've changed...?
2021-04-22 3:57 PM
Hi @Iyoon.1 ,
First let me welcome you to the STM32 Community :smiling_face_with_smiling_eyes:
Thanks for posting your feedback. I doubt that this issue is related to the STM32CubeMX tool since you're using stemwin example available in the STM32Cube firmware examples for STM32F3 Series. Please correct me if I have misunderstood.
Other topics has been added to this post, in order to increase its chance to be reviewed by our experts.
Hi @Imen DAHMEN , @Amel NASRI ,
Can you please help @Iyoon.1 and provide a status on this reported issue.
Khouloud.
2021-04-26 2:45 AM
Hello @Iyoon.1 ,
I cannot reproduce this error using IAR v8.50 when running the STemWin example with STM32CubeF3 v1.11.2:
STM32Cube_FW_F3_V1.11.2\Projects\STM32303C_EVAL\Applications\STemWin\STemWin_HelloWorld\EWARM
Which example are using ?
Can you please try to use previous version of EWARM, then keep me informed about your update.
Imen
2021-04-26 3:29 AM
Have you contacted IAR about this?
2021-04-26 4:09 PM
No problem using IAR v8.50, but I 'm using IAR v9.10.
2021-04-26 4:12 PM
The IAR has not been contacted yet because an error occurred in "stm32f3xx hal rcc.c".
2021-04-27 9:32 AM
It's their error message - so they would be the best placed to understand what, exactly, would cause it to say that.
And you say there is no error when using an earlier IAR version - so you should at least be asking IAR what they've changed...?
2021-04-30 1:13 AM
I confirmed from them that this error is an IAR IDE issue. The v9.10.2 update will be available around May 19th.
Thanks for your reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.