STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

I am using STM32L476G-DISCO board with dual usb (micro and mini). through mini I program, and through micro I want to send data. There was a problem with micro usb transfer.

good afternoon, can you tell me, I have a board with two usb (micro and mini) through the mini connector I program, and through the micro I want to send data. I fiddled with the USB Vurtual COM port implementation, tried to send string data, but the ...

0693W00000AMXxtQAH.png 0693W00000AMXyDQAX.png 0693W00000AMXxjQAH.png
DOgur.1 by Associate II
  • 2009 Views
  • 5 replies
  • 0 kudos

STMCubeIDE v1.6.1 silent failure generating peripheral files

When configuring TIM peripheral, result tim.c file has something that looks like a java runtime error dump (see attached file around line 110 and later): "FreeMarker template error (DEBUG mode; use RETHROW in production!):"Steps to reproduce this:Con...

JPard.2 by Associate
  • 882 Views
  • 0 replies
  • 0 kudos

Resolved! How to partially configure GPIO using HAL and CubeMX?

Hi,I want to partially configure GPIO's using HAL and CubeMX. In my simple case, I just want to enable/disable the pull-up resistors while running a program.At first I looked up, how the pins get initialized by CubeMX:There's this structure, which yo...

I tried configuring the SAI peripheral in STM32F469. After initialization I was unable to get any clock outputs including MCLK.

Help me in initialization.Here is the initialization i made/* SAI1 init function */void MX_SAI1_Init(void){ /* USER CODE BEGIN SAI1_Init 0 */ /* USER CODE END SAI1_Init 0 */ /* USER CODE BEGIN SAI1_Init 1 */ /* USER CODE END SAI1_Init 1 */ hsai_Block...

SNULU by Associate II
  • 2599 Views
  • 4 replies
  • 0 kudos

what is To Power???

helloI use STM23CubeMX, but i have question.what is To Power???? why to connect system clock to to power??

0693W00000AMRdnQAH.png
MYu.1 by Associate II
  • 2146 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.