2021-01-25 7:07 AM
Hi,
Looking at the STM32G4 Errata:
I see two issues regarding internal flash:
2.2.2 Data cache might be corrupted during Flash memory read-while-write operation
2.2.3 FLASH_ECCR corrupted upon reset or power-down occurring during Flash memory program or erase operation
Now I wonder if the workarounds have been somehow implemented into the CubeMX FW HAL and the X-CUBE-EEPROM package as these are directly affected by the bugs listed above. I looked through the code and release notes but could not find any hints.
Thanks in advance,
Anguel
2021-04-27 6:44 AM
Hi Anguel (Community Member),
The first errata:
2.2.2 Data cache might be corrupted during Flash memory read-while-write operation
is implemented inside the STM32Cube - disabled data cache in erase operation (see the function "HAL_FLASHEx_Erase").
Regards
Igor
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.