STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeIDE v1.7 - doesn't generate FreeRTOS files

Hello,I have installed STM32CubeIDE v1.7 and I am using STM32F746 - Discovery Board. Also I have installed the STM32F7 package v1.16.0 & 1.16.1.When I create a new project I configure my mcu parameters from STM32CubeMX which is located in the STM32Cu...

VGiot by Associate II
  • 3252 Views
  • 5 replies
  • 0 kudos

Resolved! Does RTC backup reset when power is turned off?

RTC was set in Cube MX. (0y/0M/0d 0h:0m:0s)A backup register is used to store the date and time.For example, if you press the reset button at 0/0/0 0:1:1, RTC is activated from 1m 1s.But when I turn off the power and turn on the power again, it goes ...

ckim.2390 by Associate II
  • 2111 Views
  • 1 replies
  • 0 kudos

UART communication works only in debug mode

Hi,I hope this is the right topic to ask this question.I'm new to embedded, and I'm experimenting with stm32l496ag discovery and sending/receiving uart form the connected pc using interrupts.I configured USART2 in CubeMX, enabling "global interrupt" ...

CHech.1 by Associate III
  • 4515 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.