2021-07-19 4:04 PM
Hi,
I'm using the STM32CubeIDE v1.6.1 and using FW.F2.1.9.3 firmware package with are both currently the lastest up to date versions.
Setting up an STM32CubeMX project for low layer library to be able to use RTC, the code generator is not working properly.
Here is how to generates the code:
/** Initialize RTC and set the Time and Date
*/
RTC_InitStruct.HourFormat = LL_RTC_HOURFORMAT_24HOUR;
RTC_InitStruct.AsynchPrescaler = 127;
RTC_InitStruct.SynchPrescaler = 255;
LL_RTC_Init(RTC, &RTC_InitStruct);
LL_RTC_SetAsynchPrescaler(RTC, 127);
LL_RTC_SetSynchPrescaler(RTC, 255);
/** Initialize RTC and set the Time and Date
*/
if(LL_RTC_BAK_GetRegister(RTC, LL_RTC_BKP_DR0) != 0x32F2){
RTC_TimeStruct.Hours = 0;
RTC_TimeStruct.Minutes = 50;
RTC_TimeStruct.Seconds = 0;
LL_RTC_TIME_Init(RTC, LL_RTC_FORMAT_BCD, &RTC_TimeStruct);
RTC_DateStruct.WeekDay = LL_RTC_WEEKDAY_TUESDAY;
RTC_DateStruct.Month = LL_RTC_MONTH_JULY;
RTC_DateStruct.Year = 21;
LL_RTC_DATE_Init(RTC, LL_RTC_FORMAT_BCD, &RTC_DateStruct);
LL_RTC_BAK_SetRegister(RTC,LL_RTC_BKP_DR0,0x32F2);
}But here there are two major problems which can be fixed easily by the stm32 developers:
1- Values should be written in hexadecamal format, i.e. 0x50 instead of 50.
2- "Day" is not initialized.
I changed the code as follows to fix it:
RTC_InitStruct.HourFormat = LL_RTC_HOURFORMAT_24HOUR;
RTC_InitStruct.AsynchPrescaler = 127;
RTC_InitStruct.SynchPrescaler = 255;
LL_RTC_Init(RTC, &RTC_InitStruct);
LL_RTC_SetAsynchPrescaler(RTC, 127);
LL_RTC_SetSynchPrescaler(RTC, 255);
/** Initialize RTC and set the Time and Date
*/
// if(LL_RTC_BAK_GetRegister(RTC, LL_RTC_BKP_DR0) != 0x32F2){
RTC_TimeStruct.Hours = 0x1;
RTC_TimeStruct.Minutes = 0x33;
RTC_TimeStruct.Seconds = 0x0;
LL_RTC_TIME_Init(RTC, LL_RTC_FORMAT_BCD, &RTC_TimeStruct);
RTC_DateStruct.WeekDay = LL_RTC_WEEKDAY_TUESDAY;
RTC_DateStruct.Day = 0x20;
RTC_DateStruct.Month = LL_RTC_MONTH_JULY;
RTC_DateStruct.Year = 0x21;
LL_RTC_DATE_Init(RTC, LL_RTC_FORMAT_BCD, &RTC_DateStruct);
LL_RTC_BAK_SetRegister(RTC,LL_RTC_BKP_DR0,0x32F2);
// }Also
if(LL_RTC_BAK_GetRegister(RTC, LL_RTC_BKP_DR0) != 0x32F2)statement won't return true so I had to cancel it out.
Solved! Go to Solution.
2021-07-29 12:52 AM
Hi @Ogulcan Ariyurek ,
Latest version of STM32CubeIDE is 1.7.0. Date parameter is initialized with this version. I suggest you to migrate to this version.
Regarding parameters initialization, I am not sure that they have to be written in hexadecimal format as following assert checks are applied:
#define IS_LL_RTC_HOUR24(__HOUR__) ((__HOUR__) <= 23U)
#define IS_LL_RTC_MINUTES(__MINUTES__) ((__MINUTES__) <= 59U)
#define IS_LL_RTC_SECONDS(__SECONDS__) ((__SECONDS__) <= 59U)-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-07-29 12:52 AM
Hi @Ogulcan Ariyurek ,
Latest version of STM32CubeIDE is 1.7.0. Date parameter is initialized with this version. I suggest you to migrate to this version.
Regarding parameters initialization, I am not sure that they have to be written in hexadecimal format as following assert checks are applied:
#define IS_LL_RTC_HOUR24(__HOUR__) ((__HOUR__) <= 23U)
#define IS_LL_RTC_MINUTES(__MINUTES__) ((__MINUTES__) <= 59U)
#define IS_LL_RTC_SECONDS(__SECONDS__) ((__SECONDS__) <= 59U)-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-08-26 2:02 AM
Thanks @Amel NASRI ,
I'm currently dealing with another problem, but I will check and report my results ASAP.
Regards,
Ogulcan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.