STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Invalid usbd_conf.c generated by STM32Cube v6.3.0

Output in the usbd_conf.c file when generating code for a CDC device. Code is using USE_HAL_PCD_REGISTER_CALLBACK for HAL_PCD_MspInit and HAL_PCD_MspDeInit instead of USE_HAL_PCD_REGISTER_CALLBACKS (note the final 'S'), which was there in previous ve...

0693W00000DqNvGQAV.png
pbk by Associate
  • 2139 Views
  • 4 replies
  • 0 kudos

Is it possible to use the internal OPAMP from the STM32G4 series with only the VINPx pin assigned to a physical pin? Configured as non-inverting, negative feedback with a gain.

I would like to implement a current sensing using a grounded shunt resistor. Therefore I would like to use the build-in OPAMP from the STM32G491 Series. But I'm not satisfied with the CubeMX configuration.In AN5306 I found a configuration under 4.4.1...

MWält.2 by Associate II
  • 2452 Views
  • 3 replies
  • 1 kudos

Resolved! How do I report an error in Cube initialization code?

I am using stm32L412CBU microcontroller and I am using both ADC units. The code generation generates this line of code:PeriphClkInit.AdcClockSelection = ADCCLockSelection; which is incorrect according to the structure RCC_PeriphCLKInitTypeDef for th...

MKass.1 by Associate II
  • 1809 Views
  • 2 replies
  • 0 kudos

Same pin as timer input and GPIO input

If I configure a pin as a timer input capture channel input, can I also read the state of that pin as a GPIO input?I'd like configure the timer channel as an input capture channel, and I'd like to capture both rising and falling edges. But when the e...

AJame.1 by Associate II
  • 4167 Views
  • 3 replies
  • 1 kudos

Why time input capture does not work continiously?

Hello everyone. I am working on a project that measures the duty cycle of the signal. I've initialized timer 1 as an input capture mode to measure the pulse width of a signal. Both input capture 1 and input capture 2 are used to signal the rising and...

AKhor.1 by Associate II
  • 3017 Views
  • 5 replies
  • 0 kudos

I am trying to use NUCLEO 1444 H7 LEGACY to config and run ethernet LWIP from the 1.8.0 version of the STM32H7 firmware at STM32Cube_FW_H7_V1.8.0 and the 6.0 version of the CubeMX.But it cannot work. We also run demo code ,it is ok.

Hi,there. I am trying to run LWIP on the Nucleo-H723ZG development board and cannot get any response to ping.  If I attach the debugger, STM32 can receive ARP requests and cannt send out ARP responses. When I use computer ping STM32 attarchin...

KJame.1 by Associate II
  • 1211 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to use package creator MX

Hi�?​I want to import cellular software expansion by package creator. However, it shows that JAVA FX is missing in the run time environment. Even, I have re-installed STM32 MX again. Any solution to solve this issue?

0693W00000DlXg1QAF.png
ZWH.1 by Associate II
  • 961 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.